PF0200 interrupt handler in Yocto 3.10

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

PF0200 interrupt handler in Yocto 3.10

850 次查看
davesimonson
Contributor I

How do I use/handle the INTB interrupt from the PF0200 PMIC in Yocto 3.10?

标签 (4)
0 项奖励
回复
1 回复

765 次查看
igorpadykov
NXP Employee
NXP Employee

Hi DAVE

INTB interrupt could be used as fault event, like pmic overheating or

overcurrent described in Table 100. Interrupt, Mask and Sense Bits

MMPF0200 Datasheet

http://cache.freescale.com/files/analog/doc/data_sheet/MMPF0200.pdf

Seems currently this interrupt is not used in linux.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复