PF0200 interrupt handler in Yocto 3.10

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

PF0200 interrupt handler in Yocto 3.10

868件の閲覧回数
davesimonson
Contributor I

How do I use/handle the INTB interrupt from the PF0200 PMIC in Yocto 3.10?

ラベル(4)
0 件の賞賛
返信
1 返信

783件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi DAVE

INTB interrupt could be used as fault event, like pmic overheating or

overcurrent described in Table 100. Interrupt, Mask and Sense Bits

MMPF0200 Datasheet

http://cache.freescale.com/files/analog/doc/data_sheet/MMPF0200.pdf

Seems currently this interrupt is not used in linux.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信