PF0100A OTP

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
2,176件の閲覧回数
satoshishimoda
Senior Contributor I

Hi community,

I have a question about PF0100A OTP.

Please see Table 2 in MMPF0100 datasheet (Rev.7.0).

It says "It is required to set FUSE_POR1, FUSE_POR2, and FUSE_POR3 bits during OTP programming." in description of OTP_FUSE_PORx register setting during OTP programming.

I understand user should note this difference only when using MMPF0100NPAxx.

On the other hand, all MMPF0100FxAxx OTP is programmed before shipping, so FUSE_PORx bits have already been set to "1" for MMPF0100FxAxx when user get the chip.

So user can ignore this difference when using MMPF0100FxAxx.

Is my understanding correct?

Best Regards,

Satoshi Shimoda

タグ(2)
1 解決策
1,954件の閲覧回数
Joshevelle
Senior Contributor I

Hello Satoshi,

You´re correct, the OTP_FUSE_PORx only applies for the PF0100 and PF0100A, the MMPF0100Fxxxx is already factory programmed, hence the final user can ignore table 2 since it only applies for  PF0100 and PF0100A, not PF0100F.

Hope it helps!

Josh

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,955件の閲覧回数
Joshevelle
Senior Contributor I

Hello Satoshi,

You´re correct, the OTP_FUSE_PORx only applies for the PF0100 and PF0100A, the MMPF0100Fxxxx is already factory programmed, hence the final user can ignore table 2 since it only applies for  PF0100 and PF0100A, not PF0100F.

Hope it helps!

Josh

0 件の賞賛
返信
1,954件の閲覧回数
jamesbone
NXP TechSupport
NXP TechSupport

Joshevelle, Can you please comment?