PF0100 OTP version F1 vs. F3

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PF0100 OTP version F1 vs. F3

2,055 Views
jhones
Contributor I

Hi,

Regarding the OTP options F1/F3. In the datasheet it says: "For designs using the i.MX6 Solo Lite, it is recommended to use the F3 OTP option instead of the F1 OTP option" does that apply for imx6 quad/dual processor as well?

i.e. for a Quad/Dual design can I use a F1 OTP or should I use only F3 since F3 is the corrected version?

thanks,

jhones

Labels (3)
0 Kudos
Reply
2 Replies

1,852 Views
loichureau
NXP Employee
NXP Employee

Hello,

F0A programming is for DDR3 1.5V (on SW3), if you are using DDR3L 1.35V you can use the PF0100F6A.

You have the starting sequence of each programming detailed in table 10 of the datasheet.

Best regards,

Loic

0 Kudos
Reply

1,852 Views
igorpadykov
NXP Employee
NXP Employee

Hi J H

no, this note is only for i.MX6 Solo Lite design, for a Quad/Dual it is

F0 OTP , Table 1 Orderable Part Variations  MMPF0100 .

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply