PF0100 OTP version F1 vs. F3

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

PF0100 OTP version F1 vs. F3

2,062件の閲覧回数
jhones
Contributor I

Hi,

Regarding the OTP options F1/F3. In the datasheet it says: "For designs using the i.MX6 Solo Lite, it is recommended to use the F3 OTP option instead of the F1 OTP option" does that apply for imx6 quad/dual processor as well?

i.e. for a Quad/Dual design can I use a F1 OTP or should I use only F3 since F3 is the corrected version?

thanks,

jhones

ラベル(3)
0 件の賞賛
返信
2 返答(返信)

1,859件の閲覧回数
loichureau
NXP Employee
NXP Employee

Hello,

F0A programming is for DDR3 1.5V (on SW3), if you are using DDR3L 1.35V you can use the PF0100F6A.

You have the starting sequence of each programming detailed in table 10 of the datasheet.

Best regards,

Loic

0 件の賞賛
返信

1,859件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi J H

no, this note is only for i.MX6 Solo Lite design, for a Quad/Dual it is

F0 OTP , Table 1 Orderable Part Variations  MMPF0100 .

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信