PF0100 Default configuration

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PF0100 Default configuration

1,375 Views
houdenglv
Contributor I

PWRON signal is used to turn on PMIC. It can be configured to detect a level, or an edge using the PWRON_CFG
bit as below. What's the default configuration of PWRON_CFG? 0 or 1?

pastedImage_2.png

Labels (1)
Tags (1)
0 Kudos
Reply
1 Reply

1,236 Views
igorpadykov
NXP Employee
NXP Employee

Hi Devin

default fuse state is unprogrammed, 0.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------