PF0100 Default configuration

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

PF0100 Default configuration

1,376 次查看
houdenglv
Contributor I

PWRON signal is used to turn on PMIC. It can be configured to detect a level, or an edge using the PWRON_CFG
bit as below. What's the default configuration of PWRON_CFG? 0 or 1?

pastedImage_2.png

标签 (1)
标记 (1)
0 项奖励
回复
1 回复

1,237 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Devin

default fuse state is unprogrammed, 0.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------