PF0100 Charging Issue

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

PF0100 Charging Issue

1,497件の閲覧回数
Jochi119
Contributor II

Hello,

I have the SABRE SDB and I placed a coin cell battery on the board, but it doesn't charge the battery.  When the battery is initially placed (with a charge) the RTC works as intended, but when battery discharges and power is plugged in, the PF0100 is not charging.  Could it be that by default the PF0100 does not have the COINCHEN bit enabled in the COINCTL register?

Joseph

ラベル(1)
0 件の賞賛
返信
1 返信

1,414件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Joseph

yes you are right, also one needs to set VCOIN -Coin cell charger output voltage

1.jpg

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信