PF0100 Charging Issue

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PF0100 Charging Issue

1,510 Views
Jochi119
Contributor II

Hello,

I have the SABRE SDB and I placed a coin cell battery on the board, but it doesn't charge the battery.  When the battery is initially placed (with a charge) the RTC works as intended, but when battery discharges and power is plugged in, the PF0100 is not charging.  Could it be that by default the PF0100 does not have the COINCHEN bit enabled in the COINCTL register?

Joseph

Labels (1)
0 Kudos
Reply
1 Reply

1,427 Views
igorpadykov
NXP Employee
NXP Employee

Hi Joseph

yes you are right, also one needs to set VCOIN -Coin cell charger output voltage

1.jpg

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply