PCM setting on imx8

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

PCM setting on imx8

6,627 次查看
jimi_lin
Contributor I

HI NXP

I had issue a question of this topic, but I can't replay it anymore, so I re-create it here.

I had create a sound card for PCM(SAI2) on IMX8. (SAI2 PCM connect to BT module).

We use android OS with tinyalsa on it.

And we can see the waveform on the scope, there is clk, sync and output data(TX) on SAI2 after issue cmd "tinyplay chirp.wav -D 3 -d 0" (bluetooth sound card is 3 on SAI2).

Then we set the BT module to PCM loopback mode.

After set the BT module to PCM loopback mode, we can see the input data on PCM RX.

But when we use tinycap(tinycap test.wav -D 3 -d 0 -c 1 -r 8000) to record the RX data, we just got the .wav header with dummy data(0).

Did I miss any setting on the audio driver or device tree? Below is the device tree of my bluetooth sound card on SAI2 PCM.

+        btsco_codec: btsco_codec@0 {
+                compatible= "linux,bt-sco";
+                status = "okay";
+        };
+        sound-btsco {
+
+                compatible = "fsl,imx-audio-btsco";
+                model = "btsco-codec";
+                audio-cpu = <&sai2>;
+                btsco-controller = <&btsco_codec>;
+
+        };

+&sai2 {
+        pinctrl-names = "default";
+        pinctrl-0 = <&pinctrl_sai2>;
+        assigned-clocks = <&clk IMX8MM_CLK_SAI2>;
+        assigned-clock-parents = <&clk IMX8MM_AUDIO_PLL1_OUT>;
+        assigned-clock-rates = <24576000>;
+        status = "okay";
+};

+        pinctrl_sai2: sai2grp {
+                fsl,pins = <
+                         MX8MM_IOMUXC_SAI2_TXFS_SAI2_TX_SYNC             0xd6
+                         MX8MM_IOMUXC_SAI2_TXC_SAI2_TX_BCLK              0xd6
+                         MX8MM_IOMUXC_SAI2_RXD0_SAI2_RX_DATA0            0xd6
+                         MX8MM_IOMUXC_SAI2_TXD0_SAI2_TX_DATA0            0xd6
+                >;
+        };

 

Thanks

0 项奖励
回复
10 回复数

6,472 次查看
jimi_lin
Contributor I

HI igorpadykov

"by "SYNC output" - what i.MX8MM signal do you mean ?"

->MX8MM_IOMUXC_SAI2_TXFS_SAI2_TX_SYNC

And in the fsl_sai.c, which kind of synchronous mode should i set? sai-synchronous-rx or sai-asynchronous?

I'm not sure the meaning of "synchronous mode".

Thanks

0 项奖励
回复

6,472 次查看
jimi_lin
Contributor I

HI igorpadykov

When I config the cpu_dai format to master as below, I can generate the CLK and also see the TX data while tinyplay exec.

But I can't see the SYNC output, did I miss any config? 

ret = snd_soc_dai_set_fmt(cpu_dai, SND_SOC_DAI_FORMAT_DSP_A
                 | SND_SOC_DAIFMT_NB_NF | SND_SOC_DAIFMT_CBS_CFS | SND_SOC_DAIFMT_CONT);

Thanks

0 项奖励
回复

6,472 次查看
igorpadykov
NXP Employee
NXP Employee

by "SYNC output" - what i.MX8MM signal do you mean ?

Best regards
igor

0 项奖励
回复

6,472 次查看
jimi_lin
Contributor I

HI igorpadykov

There is PCM in below section 3.5

https://www.nxp.com/docs/en/application-note/AN12202.pdf

And it's also mentioned in below community

https://community.nxp.com/thread/524538

So, how do I config the SAI2 to above PCM interface/format? Or I can just config it to I2S/TDM?

Thanks

0 项奖励
回复

6,472 次查看
jimi_lin
Contributor I

HI igorpadykov 

Does the SAI2 can config to PCM interface? Or just I2S?

Thanks

0 项奖励
回复

6,472 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Jimi

 

>Does the SAI2 can config to PCM interface?

"PCM"  is general meaning, so you should always check external chip

documentation for its interface timings.

 

Best regards
igor

0 项奖励
回复

6,472 次查看
jimi_lin
Contributor I

HI igorpadykov

We can see the wavform on the scope on PCM RX.

Is there any method to see the real value on SAI2(PCM) RX.

Thanks

0 项奖励
回复

6,472 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Jimi

 

>Is there any method to see the real value on SAI2(PCM) RX.

seems only by oscilloscope or reading SAI Receive FIFO Register RFR.

 

Best regards
igor

0 项奖励
回复

6,472 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Jimi

one can try to narrow down issue and test loop back PCM(SAI2)

without BT module, to check if issue is caused by BT module or i.MX.

For android OS with tinyalsa usage may be helpful:

VAR-SOM-MX6 Android Unit Testing - Variscite Wiki 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

6,472 次查看
jimi_lin
Contributor I

HI igorpadykov

Does the setting of SAI2 to PCM correct(in devtree)? Or?

We use this 4 pins

MX8MM_IOMUXC_SAI2_TXFS_SAI2_TX_SYNC   <-> PCM_SYNC
MX8MM_IOMUXC_SAI2_TXC_SAI2_TX_BCLK     <-> PCM_CLK         
MX8MM_IOMUXC_SAI2_RXD0_SAI2_RX_DATA0<-> PCM_OUT
MX8MM_IOMUXC_SAI2_TXD0_SAI2_TX_DATA0 <-> PCM_IN

Thanks

0 项奖励
回复