PCM/I2S support on imx6q

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

PCM/I2S support on imx6q

1,319 次查看
bikash
Contributor II

Hi,

On our custom board, we are going to use a codec which gives PCM output.

Please let us know in perspective of IMX6Q processor, how PCM differs from I2S.

At many places, it is mentioned that PCM is similar to I2S.

Could  we use the same "ssi interface" driver  for  both PCM & I2S.

Thanks,

Bikash

标签 (2)
0 项奖励
回复
2 回复数

1,131 次查看
sumit8915
Contributor III

Hi Bikas,

Have to come to any conclusion regarding this?

Thanks

Sumit

0 项奖励
回复

1,131 次查看
igorpadykov
NXP Employee
NXP Employee

Hi bikash

"PCM" word is too generic and vague to provide accurate answer,

some PCM formats may be supported, some not.

Suggest to check codec datasheet and compare with i.MX6 RM SSI chapter

to understand if it can be supported.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复