PCIe link timeout issue on iMX6Q smart device board

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

PCIe link timeout issue on iMX6Q smart device board

跳至解决方案
1,887 次查看
pingchuanma
Contributor I

Hi experts,

The SDK PCIe test fails on iMX6Q smart_device board. It shows:

Please make sure the mini pcie card inserted. Type"y" or "Y" to confirm.
Link timeout.
PCIE init failed.

Was the PCIe source code validated on iMX6Q smart device board? Thanks a lot.

标签 (1)
0 项奖励
回复
1 解答
1,688 次查看
igorpadykov
NXP Employee
NXP Employee

Hi pingchuan,

SDK works well please refer to attached file (based on SDK).

You can try other card.

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,689 次查看
igorpadykov
NXP Employee
NXP Employee

Hi pingchuan,

SDK works well please refer to attached file (based on SDK).

You can try other card.

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复
1,688 次查看
pingchuanma
Contributor I

The board is smart_device_rev_c

0 项奖励
回复