PCIe link timeout issue on iMX6Q smart device board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PCIe link timeout issue on iMX6Q smart device board

Jump to solution
1,880 Views
pingchuanma
Contributor I

Hi experts,

The SDK PCIe test fails on iMX6Q smart_device board. It shows:

Please make sure the mini pcie card inserted. Type"y" or "Y" to confirm.
Link timeout.
PCIE init failed.

Was the PCIe source code validated on iMX6Q smart device board? Thanks a lot.

Labels (1)
0 Kudos
Reply
1 Solution
1,681 Views
igorpadykov
NXP Employee
NXP Employee

Hi pingchuan,

SDK works well please refer to attached file (based on SDK).

You can try other card.

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
2 Replies
1,682 Views
igorpadykov
NXP Employee
NXP Employee

Hi pingchuan,

SDK works well please refer to attached file (based on SDK).

You can try other card.

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
1,681 Views
pingchuanma
Contributor I

The board is smart_device_rev_c

0 Kudos
Reply