PCIe hot-plug iMX8MM Support

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

PCIe hot-plug iMX8MM Support

4,615 次查看
raajeshk88
Contributor III

Hi,

      Does iMX8MM support PCIe hot-plug? I saw some previous questions about iMX6 which had contradicting answers as it supports and not supports. Regarding iMX8 https://community.nxp.com/thread/494660  this shows as it does not support but RM shows the registers for hot plug. Could you pleaase help to clarify this since we are in a time crunch for a proposal. Thanks

0 项奖励
回复
5 回复数

4,524 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Raajesh

 

unfortunately hardware does not supports it.

 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

4,524 次查看
raajeshk88
Contributor III

Hi Igor,

       Thanks for the reply. There is no reference examples but the standard PCIe BSP has the feature enabled. Is my understanding correct.

Regards,

Raajesh K

0 项奖励
回复

4,524 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Raajesh

 

yes standard PCIe BSP is enabled, except PCIe hot-plug.

 

Best regards
igor

0 项奖励
回复

4,231 次查看
zhangjunsheng
Contributor III

Hi Igor:

 

     How can we verify the PCIe hotplug feature/support by using the NXP demo board (imx8mm-evk)?

 

Best regards.

Johnson

0 项奖励
回复

4,185 次查看
weidong_sun
NXP TechSupport
NXP TechSupport

I confirmed it with i.mx expert hardware team again.

So clarify it again. 

Hardware: PCIe interface doesn't support Hot plug.

software:  Not support Hot plug, too.

 

DON'T USE HOT PLUG feature of PCIe On i.MX8MM.

Up to now, PCIe interface of all imx processors(i.MX6/7/8) doesn't support Hot plug.

 

Have a nice day!

B.R,

Weidong