PCIe hot-plug iMX8MM Support

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

PCIe hot-plug iMX8MM Support

4,602件の閲覧回数
raajeshk88
Contributor III

Hi,

      Does iMX8MM support PCIe hot-plug? I saw some previous questions about iMX6 which had contradicting answers as it supports and not supports. Regarding iMX8 https://community.nxp.com/thread/494660  this shows as it does not support but RM shows the registers for hot plug. Could you pleaase help to clarify this since we are in a time crunch for a proposal. Thanks

ラベル(2)
0 件の賞賛
返信
5 返答(返信)

4,511件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Raajesh

 

unfortunately hardware does not supports it.

 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

4,511件の閲覧回数
raajeshk88
Contributor III

Hi Igor,

       Thanks for the reply. There is no reference examples but the standard PCIe BSP has the feature enabled. Is my understanding correct.

Regards,

Raajesh K

0 件の賞賛
返信

4,511件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Raajesh

 

yes standard PCIe BSP is enabled, except PCIe hot-plug.

 

Best regards
igor

0 件の賞賛
返信

4,218件の閲覧回数
zhangjunsheng
Contributor III

Hi Igor:

 

     How can we verify the PCIe hotplug feature/support by using the NXP demo board (imx8mm-evk)?

 

Best regards.

Johnson

0 件の賞賛
返信

4,172件の閲覧回数
weidong_sun
NXP TechSupport
NXP TechSupport

I confirmed it with i.mx expert hardware team again.

So clarify it again. 

Hardware: PCIe interface doesn't support Hot plug.

software:  Not support Hot plug, too.

 

DON'T USE HOT PLUG feature of PCIe On i.MX8MM.

Up to now, PCIe interface of all imx processors(i.MX6/7/8) doesn't support Hot plug.

 

Have a nice day!

B.R,

Weidong