PCIe WiFi for iMX6

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
3,524件の閲覧回数
bfac
NXP Employee
NXP Employee

Hello!

Do you have a reference of PCIe WiFi card that is known to work with iMX6Q on the SABRE-SD board?

Would you know if the required BSP porting efforts are high for that module based on the FSL BSP?

A customer is looking for higher throughput on the WiFi connection than the actual used solution over SDIO.

Thanks!

Bruno

ラベル(3)
タグ(3)
0 件の賞賛
返信
1 解決策
2,447件の閲覧回数
FrankLi1z
NXP Employee
NXP Employee

You can use intel iwl4965.

If you use above wifi card, needn't port. Kernel already supported it.

If you use other wifi card, need thirdpart provide wifi card driver.

best regards

Frank Li

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,448件の閲覧回数
FrankLi1z
NXP Employee
NXP Employee

You can use intel iwl4965.

If you use above wifi card, needn't port. Kernel already supported it.

If you use other wifi card, need thirdpart provide wifi card driver.

best regards

Frank Li

0 件の賞賛
返信