PCIe WiFi for iMX6

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PCIe WiFi for iMX6

Jump to solution
3,512 Views
bfac
NXP Employee
NXP Employee

Hello!

Do you have a reference of PCIe WiFi card that is known to work with iMX6Q on the SABRE-SD board?

Would you know if the required BSP porting efforts are high for that module based on the FSL BSP?

A customer is looking for higher throughput on the WiFi connection than the actual used solution over SDIO.

Thanks!

Bruno

Labels (3)
Tags (3)
0 Kudos
Reply
1 Solution
2,435 Views
FrankLi1z
NXP Employee
NXP Employee

You can use intel iwl4965.

If you use above wifi card, needn't port. Kernel already supported it.

If you use other wifi card, need thirdpart provide wifi card driver.

best regards

Frank Li

View solution in original post

0 Kudos
Reply
1 Reply
2,436 Views
FrankLi1z
NXP Employee
NXP Employee

You can use intel iwl4965.

If you use above wifi card, needn't port. Kernel already supported it.

If you use other wifi card, need thirdpart provide wifi card driver.

best regards

Frank Li

0 Kudos
Reply