PCIe WiFi for iMX6

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

PCIe WiFi for iMX6

跳至解决方案
3,529 次查看
bfac
NXP Employee
NXP Employee

Hello!

Do you have a reference of PCIe WiFi card that is known to work with iMX6Q on the SABRE-SD board?

Would you know if the required BSP porting efforts are high for that module based on the FSL BSP?

A customer is looking for higher throughput on the WiFi connection than the actual used solution over SDIO.

Thanks!

Bruno

标签 (3)
标记 (3)
0 项奖励
回复
1 解答
2,452 次查看
FrankLi1z
NXP Employee
NXP Employee

You can use intel iwl4965.

If you use above wifi card, needn't port. Kernel already supported it.

If you use other wifi card, need thirdpart provide wifi card driver.

best regards

Frank Li

在原帖中查看解决方案

0 项奖励
回复
1 回复
2,453 次查看
FrankLi1z
NXP Employee
NXP Employee

You can use intel iwl4965.

If you use above wifi card, needn't port. Kernel already supported it.

If you use other wifi card, need thirdpart provide wifi card driver.

best regards

Frank Li

0 项奖励
回复