PCIE-EP GEN3 support

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

PCIE-EP GEN3 support

2,810件の閲覧回数
deepakraj
Contributor III

Hi ,

we have successfully enabled PCIE-EP configuration in our IMX8MP module and PCIE-EP device can detect in PCIE-RC(IMX8MP) device also.
But it was detected only as GEN1 Speed 2.5GT/s, Width x1. 

We have enabled dts changes " max-link-speed = <3>;"  in EP & RC kernel. But no change in PCIE GEN speed.

Refer below lspci command output of PCIE-EP Device

root@lec-imx8mp:~# lspci -s 01:00.0 -vv
01:00.0 Unassigned class [ff00]: Freescale Semiconductor Inc Device 81c0
Control: I/O- Mem+ BusMaster+ SpecCycle- MemWINV- VGASnoop- ParErr- Stepping- SERR- FastB2B- DisINTx+
Status: Cap+ 66MHz- UDF- FastB2B- ParErr- DEVSEL=fast >TAbort- <TAbort- <MAbort- >SERR- <PERR- INTx-
Latency: 0
Interrupt: pin A routed to IRQ 237
Region 0: Memory at 18100000 (32-bit, non-prefetchable) [size=64K]
Region 2: Memory at 18110000 (32-bit, non-prefetchable) [size=64K]
Region 4: Memory at 18130000 (32-bit, non-prefetchable) [size=256]
Region 5: Memory at 18120000 (32-bit, non-prefetchable) [size=64K]
Expansion ROM at 18200000 [virtual] [disabled] [size=64K]
Capabilities: [40] Power Management version 3
Flags: PMEClk- DSI- D1+ D2- AuxCurrent=375mA PME(D0+,D1+,D2-,D3hot+,D3cold+)
Status: D0 NoSoftRst- PME-Enable- DSel=0 DScale=0 PME-
Capabilities: [50] MSI: Enable+ Count=16/16 Maskable+ 64bit+
Address: 0000000045818000 Data: 0010
Masking: 00000000 Pending: 00000000
Capabilities: [70] Express (v2) Endpoint, IntMsgNum 0
DevCap: MaxPayload 128 bytes, PhantFunc 0, Latency L0s <64ns, L1 <1us
ExtTag- AttnBtn- AttnInd- PwrInd- RBE+ FLReset- SlotPowerLimit 0W
DevCtl: CorrErr- NonFatalErr- FatalErr- UnsupReq-
RlxdOrd+ ExtTag- PhantFunc- AuxPwr- NoSnoop-
MaxPayload 128 bytes, MaxReadReq 512 bytes
DevSta: CorrErr- NonFatalErr- FatalErr- UnsupReq- AuxPwr+ TransPend-
LnkCap: Port #0, Speed 2.5GT/s, Width x1, ASPM L0s L1, Exit Latency L0s <1us, L1 unlimited
ClockPM- Surprise- LLActRep- BwNot- ASPMOptComp+
LnkCtl: ASPM Disabled; RCB 64 bytes, LnkDisable- CommClk+
ExtSynch- ClockPM- AutWidDis- BWInt- AutBWInt-
LnkSta: Speed 2.5GT/s, Width x1
TrErr- Train- SlotClk+ DLActive- BWMgmt- ABWMgmt-
DevCap2: Completion Timeout: Range ABCD, TimeoutDis+ NROPrPrP- LTR-
10BitTagComp- 10BitTagReq- OBFF Not Supported, ExtFmt- EETLPPrefix-
EmergencyPowerReduction Not Supported, EmergencyPowerReductionInit-
FRS- TPHComp- ExtTPHComp-
AtomicOpsCap: 32bit- 64bit- 128bitCAS-
DevCtl2: Completion Timeout: 50us to 50ms, TimeoutDis-
AtomicOpsCtl: ReqEn-
IDOReq- IDOCompl- LTR- EmergencyPowerReductionReq-
10BitTagReq- OBFF Disabled, EETLPPrefixBlk-
LnkCap2: Supported Link Speeds: 2.5GT/s, Crosslink- Retimer- 2Retimers- DRS-
LnkCtl2: Target Link Speed: 8GT/s, EnterCompliance- SpeedDis-
Transmit Margin: Normal Operating Range, EnterModifiedCompliance- ComplianceSOS-
Compliance Preset/De-emphasis: -6dB de-emphasis, 0dB preshoot
LnkSta2: Current De-emphasis Level: -3.5dB, EqualizationComplete- EqualizationPhase1-
EqualizationPhase2- EqualizationPhase3- LinkEqualizationRequest-
Retimer- 2Retimers- CrosslinkRes: unsupported
Capabilities: [100 v2] Advanced Error Reporting
UESta: DLP- SDES- TLP- FCP- CmpltTO- CmpltAbrt- UnxCmplt- RxOF- MalfTLP- ECRC- UnsupReq- ACSViol-
UEMsk: DLP- SDES- TLP- FCP- CmpltTO- CmpltAbrt- UnxCmplt- RxOF- MalfTLP- ECRC- UnsupReq- ACSViol-
UESvrt: DLP+ SDES+ TLP- FCP+ CmpltTO- CmpltAbrt- UnxCmplt- RxOF+ MalfTLP+ ECRC- UnsupReq- ACSViol-
CESta: RxErr- BadTLP- BadDLLP- Rollover- Timeout- AdvNonFatalErr-
CEMsk: RxErr- BadTLP- BadDLLP- Rollover- Timeout- AdvNonFatalErr+
AERCap: First Error Pointer: 00, ECRCGenCap+ ECRCGenEn- ECRCChkCap+ ECRCChkEn-
MultHdrRecCap- MultHdrRecEn- TLPPfxPres- HdrLogCap-
HeaderLog: 00000000 00000000 00000000 00000000
Capabilities: [148 v1] Secondary PCI Express
LnkCtl3: LnkEquIntrruptEn- PerformEqu-
LaneErrStat: 0
Capabilities: [158 v1] L1 PM Substates
L1SubCap: PCI-PM_L1.2+ PCI-PM_L1.1+ ASPM_L1.2- ASPM_L1.1+ L1_PM_Substates+
PortCommonModeRestoreTime=10us PortTPowerOnTime=10us
L1SubCtl1: PCI-PM_L1.2- PCI-PM_L1.1- ASPM_L1.2- ASPM_L1.1-
T_CommonMode=0us
L1SubCtl2: T_PwrOn=10us
Kernel driver in use: pci-endpoint-test

Please share changes to update to GEN 3.

Thanks

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

2,780件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

The MX8Mplus provide GEN3 PCI just adjust the functionality:

https://community.nxp.com/pwmxy87654/attachments/pwmxy87654/imx-processors/195745/1/AN13164%20-%20iM...

 

Regards

0 件の賞賛
返信

2,731件の閲覧回数
deepakraj
Contributor III
Hi

our test connection are as below.
• i.MX 8M Plus - End Point ↔ i.MX 8M Plus – Root Complex

we checked the document, we belive we have connected IMX8MP as DUT - DUT and we got Throughput as follows using pcietest command
pcitest -r -s 8192000;
pcitest -w -s 8192000;

WRITE - 2.84 MB/s
READ - 36 MB/s
0 件の賞賛
返信