PCA9450 I2C voltage levels

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

PCA9450 I2C voltage levels

跳至解决方案
1,245 次查看
Anand97
Contributor I

Hi,

We are designing i.MX8MN based development board where the I2C bank voltage is fixed to 3.3V due to other sensor modules working at 3.3V. But as per PMIC datasheet, I2C lines are operating at 1.8V. So we wanted to know if the PMIC I2C is capable of operating at 3.3V?

Also we found that the PMIC has a on-chip level translator which was used for 3.3V to 1.8V conversion in reference designs so, whether we can use that as a bridge between PMIC and processor?   

Let us know how to solve this issue.

Thanks in advance.

0 项奖励
回复
1 解答
1,237 次查看
florian_arndt
Senior Contributor I

Hello Anand,
regarding your first question ("So we wanted to know if the PMIC I2C is capable of operating at 3.3V?") I can assure you that it is possible to use 3.3V I2C to communicate with the PMIC. We use the same method in our design without problems since 2020.

Unfortunately I can't help you with the integrated level translator as I have no experience with it. Maybe someone else can help you with this.

Best regards.

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,238 次查看
florian_arndt
Senior Contributor I

Hello Anand,
regarding your first question ("So we wanted to know if the PMIC I2C is capable of operating at 3.3V?") I can assure you that it is possible to use 3.3V I2C to communicate with the PMIC. We use the same method in our design without problems since 2020.

Unfortunately I can't help you with the integrated level translator as I have no experience with it. Maybe someone else can help you with this.

Best regards.

0 项奖励
回复
1,231 次查看
Anand97
Contributor I

Thanks for the quick response florian.

0 项奖励
回复