8MMINILPD4-EVK baseboard design

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

8MMINILPD4-EVK baseboard design

756 次查看
ashish_m
Contributor I

Hi

we are designing customized board w.r.t 8MMINILPD4-EVK board

We have following requirements:

  • 13.8V supply to power carrier board from J101 connector.
  • USB1 to connect external hard disk using type c connector.
  • USB2 interface with FT232R (USB UART IC )

Planning to remove type c connector (J302) and connect USB2 DP DN connector to FT232.

 For above requirements we have following queries

  • changes needed to be done in hardware
  • configuration to be done in IC U302,U303,U305,U306

 

0 项奖励
回复
0 回复数