Overlay frame buffer support on iMX6SL evk.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Overlay frame buffer support on iMX6SL evk.

ソリューションへジャンプ
7,400件の閲覧回数
jeminmorabia
Contributor II

Hi,

In my iMX6SL evk board I am not able to see /dev/fb1 after start up.

Do iMX6SL support overlay frame buffer? How can I enable it?

In iMX6QDL processors IPU provides overlay frame buffer support.

Thanks,

Jemin Morabia

タグ(1)
0 件の賞賛
返信
1 解決策
6,668件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

mx6sl doesn't ipu, just has EPDC controler, which doesn't support overlay.

元の投稿で解決策を見る

0 件の賞賛
返信
5 返答(返信)
6,669件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

mx6sl doesn't ipu, just has EPDC controler, which doesn't support overlay.

0 件の賞賛
返信
6,668件の閲覧回数
ramd
Contributor I

Xie,

Doesn't IMX6SL have GPU2D support with EPDC controller ?

0 件の賞賛
返信
6,664件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi Morabia,

In the documents i.MX_6SoloLite_EVK_Linux_Release_Notes.pdf and i.MX_6SoloLite_Linux_Reference_Manual.pdf you can see that "Support for screen updates from an alternate (overlay) buffer".

Here I attached them for you, please have a check. Hope this can help you.


Have a great day,
Dan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

6,664件の閲覧回数
Wlodek_D_
Senior Contributor II

Hello,

Thank you for your post, however please consider moving it to the right community place (e.g. i.MX Community ) to get it visible for active members.

For details please see general advice Where to post a Discussion? (https://community.freescale.com/docs/DOC-99909 )

Thank you for using Freescale Community.

0 件の賞賛
返信
6,664件の閲覧回数
jeminmorabia
Contributor II

Thanks Wlodek_D. for your guidance.

0 件の賞賛
返信