Overlay frame buffer support on iMX6SL evk.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Overlay frame buffer support on iMX6SL evk.

Jump to solution
7,408 Views
jeminmorabia
Contributor II

Hi,

In my iMX6SL evk board I am not able to see /dev/fb1 after start up.

Do iMX6SL support overlay frame buffer? How can I enable it?

In iMX6QDL processors IPU provides overlay frame buffer support.

Thanks,

Jemin Morabia

Tags (1)
0 Kudos
Reply
1 Solution
6,676 Views
joanxie
NXP TechSupport
NXP TechSupport

mx6sl doesn't ipu, just has EPDC controler, which doesn't support overlay.

View solution in original post

0 Kudos
Reply
5 Replies
6,677 Views
joanxie
NXP TechSupport
NXP TechSupport

mx6sl doesn't ipu, just has EPDC controler, which doesn't support overlay.

0 Kudos
Reply
6,676 Views
ramd
Contributor I

Xie,

Doesn't IMX6SL have GPU2D support with EPDC controller ?

0 Kudos
Reply
6,672 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi Morabia,

In the documents i.MX_6SoloLite_EVK_Linux_Release_Notes.pdf and i.MX_6SoloLite_Linux_Reference_Manual.pdf you can see that "Support for screen updates from an alternate (overlay) buffer".

Here I attached them for you, please have a check. Hope this can help you.


Have a great day,
Dan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

6,672 Views
Wlodek_D_
Senior Contributor II

Hello,

Thank you for your post, however please consider moving it to the right community place (e.g. i.MX Community ) to get it visible for active members.

For details please see general advice Where to post a Discussion? (https://community.freescale.com/docs/DOC-99909 )

Thank you for using Freescale Community.

0 Kudos
Reply
6,672 Views
jeminmorabia
Contributor II

Thanks Wlodek_D. for your guidance.

0 Kudos
Reply