Output 125MHz vs. 100MHz for PCIe

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Output 125MHz vs. 100MHz for PCIe

2,919件の閲覧回数
cbobek
Contributor I

Hi Community,

On our Linux 3.x kernel, our PCIe bus works and outputs 125MHz on the CLK1_P and CLK1_N pins, which is what we want.  When we migrated to the Linux 4.9 kernel, the PCIe bus works, but it outputs a 100MHz clock.

When we modified the clk-imx6q.c file to output the 125MHz clock, the clock was correct, but Linux hung during boot as shown below.  Does anybody have any suggestions on how to set this configuration up in Linux 4.9?

---------- clk-imx6q.c change ------------

    if (IS_ENABLED(CONFIG_PCI_IMX6)) {

        //clk_set_parent(clk[IMX6QDL_CLK_LVDS1_SEL], clk[IMX6QDL_CLK_SATA_REF_100M]);

        clk_set_parent(clk[IMX6QDL_CLK_LVDS1_SEL], clk[IMX6QDL_CLK_PCIE_REF_125M]);

---------- Linux 4.9 crash during boot -------------

...

io scheduler noop registered

io scheduler deadline registered

io scheduler cfq registered (default)

OF: PCI: host bridge /soc/pcie@0x01000000 ranges:

OF: PCI:   No bus range found for /soc/pcie@0x01000000, using [bus 00-ff]

OF: PCI:    IO 0x01f80000..0x01f8ffff -> 0x00000000

OF: PCI:   MEM 0x01000000..0x01efffff -> 0x01000000

Thank you,

Chris

ラベル(2)
0 件の賞賛
返信
1 返信

2,329件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

  According to the following Community thread Setting the iMX6 PCIe Clocks :

The ENET PLL (PLL6) 100 MHz (SATA) PFD output MUST be enabled in order to access

the registers in the PCIe IP block.

  The following also may be useful:

question about imx6 pcie's frequency/clock 

https://community.nxp.com/message/640518 


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信