OpenWRT u-boot ERROR: ** Unrecognized filesystem type **

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

OpenWRT u-boot ERROR: ** Unrecognized filesystem type **

2,737件の閲覧回数
petertseng
Contributor IV

Hi i.MX Community,

I'm trying to port imx6 platform on OpenWrt/LEDE.

And I use the microSD boot to get the following u-boot error message.

U-Boot 2014.04-g2dfcecc-dirty (Jan 16 2018 - 17:05:01)

CPU: Freescale i.MX6SOLO rev1.2 at 792 MHz
Reset cause: POR
Board: i.MX6-MSBOARD
DRAM: 1 GiB
board_init
MMC: FSL_SDHC: 0, FSL_SDHC: 1, FSL_SDHC: 2
In: serial
Out: serial
Err: serial
BOOT_CFG: 0x00005840
From Micro-SD
Net: board_eth_init
No ethernet found.
Hit any key to stop autoboot: 0
mmc1(part 0) is current device
** Unrecognized filesystem type **
** Unrecognized filesystem type **
Booting from net ...
No ethernet found.
No ethernet found.
Bad Linux ARM zImage magic!
MSBOARD#>

How to burn the image generated by OpenWRT / LEDE to the microSD card?

Hope for your help!

Regards,

タグ(1)
0 件の賞賛
返信
1 返信

2,358件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport
0 件の賞賛
返信