OpenVG performance of i.MX6

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

OpenVG performance of i.MX6

Jump to solution
2,294 Views
george
Senior Contributor II

Dear all,

Please let me know about OpenVG processing of MX6.

Isn't there any benchmark (materials for comparing performance) when performing the OpenVG function by 2D-GPU or 3D-GPU?

Or please let me know which is fast.

Best Regards,

George

0 Kudos
Reply
1 Solution
1,627 Views
igorpadykov
NXP Employee
NXP Employee

Hi George

these materials (though there are no much) are under NDA,

please enter Service Request ticket. Also useful link below

Freescale FTF Americas 2014 - Vivante GPU Highlights

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
3 Replies
1,628 Views
igorpadykov
NXP Employee
NXP Employee

Hi George

these materials (though there are no much) are under NDA,

please enter Service Request ticket. Also useful link below

Freescale FTF Americas 2014 - Vivante GPU Highlights

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
1,627 Views
mtx512
Contributor V
0 Kudos
Reply
1,627 Views
igorpadykov
NXP Employee
NXP Employee

Hi Jas

they are not dead, they are under NDA. :smileyhappy:

Best regards

chip

0 Kudos
Reply