OpenVG cannot rotate an Image smoothly

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

OpenVG cannot rotate an Image smoothly

1,758 次查看
ali_sarlak
Contributor III

Hello community,

When I use libOpenVG_355.so my image rotation code doesn’t run smoothly but when I use libOpenVG_3D.so the same code run smoothly, why?

Extra information :

BSP : L3.0.35

SOC: IMX6Q

Image type: VG_sRGB_565

Image size : 1132,1132

(MAX Supported size is: [In libOpenVG_355.so](8192*8192) & [In libOpenVG_3D.so](1280*1280))

Thanks,

标记 (3)
0 项奖励
回复
3 回复数

1,572 次查看
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hi Ali,

Yes, new BSP is based on 4.1.15 kernel, please check it;

i.MX6Q|i.MX 6Quad Processors|Quad Core|NXP

Regards

1,572 次查看
ali_sarlak
Contributor III

Bio_TICFSL​ thanks for your reply,

I build my app with libOpenVG_355.so  and libOpenVG.so is a link to libOpenVG_355.so the result doesn't change but about your suggestion for new BSP I just found L3.0.35 and also L3.0.101_4.1.1 is there any newer BSP?

regards

0 项奖励
回复

1,572 次查看
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hi Ali,

when you build your BSP libOpenVG.so is a softlink pointing to /usr/lib/libOpenVG_355.so.

So you have to make sure that when you compile your app you use this one (using your rootfs to link against). You have to take the decision at build time to use libOpenVG.3d or libOpenVG.2d .

Also, I suggest for a BSP upgrade and use the latest GPU drivers

regards

0 项奖励
回复