OpenSSL library for i.MX

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

OpenSSL library for i.MX

Jump to solution
2,579 Views
alextimpau
Contributor III

Hello, there is a method or the possibility to use the functionalities provided by OpenSSL library for cryptographic applications development in the world of i.MX. I read about cryptographic acceleration in the CAAM but I have not found an available documentation  for this. Thanks a lot!

0 Kudos
Reply
1 Solution
2,180 Views
Yuri
NXP Employee
NXP Employee

Hello,

  The CAAM drivers are accelerated through the CryptoDev interface,

so customers can use OpenSSL library (with hardware acceleration)

as much as the lib supports the CryptoDev interface.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
2,181 Views
Yuri
NXP Employee
NXP Employee

Hello,

  The CAAM drivers are accelerated through the CryptoDev interface,

so customers can use OpenSSL library (with hardware acceleration)

as much as the lib supports the CryptoDev interface.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply