no ppp on imx6 linux

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

no ppp on imx6 linux

2,631件の閲覧回数
tonyzhou300
Contributor I

I used fsl-arm-yocto-bsp, but after I build, no pppd in linux file system.

How can I build bsp with ppp inside.

ths

0 件の賞賛
返信
1 返信

1,815件の閲覧回数
b36401
NXP Employee
NXP Employee

Please add this command into conf/local.conf file inside your build directory:

IMAGE_INSTALL_append = " ppp"

It should help.

Have a great day,

Victor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信