Which Development board should I use?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Which Development board should I use?

1,940 次查看
munishsharma
Contributor I

Hi

    I am mentioning my requirement. which board should i use which Fulfil all my requirement.

  1. Dual analog video (CVBS) input ports with parallel operations (BT656 and CSI2).

  2. Micro SD, eMMC , SATA Device for storing data.

  3. Processor IMX6.

  4. Audio in and out interfaces.

  5. Video out interfaces (HDMI)

  6. 5” or 7” LCD interface (Maximum Resolution).

  7. IR Interface for Remote control.

  8. WIFI , Ethernet and for video stemming.

  9. Bluetooth for the control.

  10. Uncompressed video storage.

  11. Rechargeable battery powered.

  12. USB Interface for transferring the data stored in flash in PC/Laptop.

  13. Capacitive Touch screen or keypad interface for control functionality

 

     do also suggest me if there is an requirement of addition module

     Thanks in Advance

    

     Regards

     Munish sharma

0 项奖励
回复
3 回复数

1,892 次查看
saurabh206
Senior Contributor III

Hi Munish

CPU board is i.MX6 board.

While base board can i.MX53 or i.MX6

MCIMX-LVDS1 LCD will work reference board.

Thanks

Saurabh

0 项奖励
回复

1,892 次查看
munishsharma
Contributor I

Hi Saurab

thanks for your suggestion.

I am confused regarding the following.

1)  In the link, they have given 1 cpu card and 1 main board. Do I have to buy both or only the main board enough for development?

2) Also can we use all the three analog video ports simultaneously?

3). can you suggest suitable LCD module with capacitive touch screen for use with this board?

thanks in Advance

regards

Munish

0 项奖励
回复

1,892 次查看
saurabh206
Senior Contributor III

Hi

Munish

You can use following board for your development.

SABRE|Automotive-Infotainment|i.MX6|Freescale

Thanks

Saurabh

0 项奖励
回复