OpenSSL Library for Linux imx

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

OpenSSL Library for Linux imx

2,481件の閲覧回数
westbrook
Contributor III

Hi guys:

I am trying to use latest openssl library(1.1.0h) in Linux imx6 bsp, how include that.

Do you have recipes to include the latest openssl.

In openssl website I see latest is openssl.1.1.0h

 

Currently I see we are using openssl.1.0.2k in linux bsp for imx6solo.

 

I tried specifying  preferred version in .config file of timesys project, I get building errors.

Thank you in advance.

ラベル(1)
タグ(2)
0 件の賞賛
返信
1 返信

2,209件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi xiao

for openssl usage one can look on

https://community.nxp.com/thread/309499 

http://events17.linuxfoundation.org/sites/events/files/slides/2017-02%20-%20ELC%20-%20Hudson%20-%20L... 

ventana/encryption – Gateworks 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信