OpenGL application development on i.MX6

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

OpenGL application development on i.MX6

3,084件の閲覧回数
frankchenmh
Contributor III

Hi,

I want to develop OpenGL application based on i.MX6 L3.0.35 linux BSP. I know there is gpu-viv-bin-mx6q in the BSP release package and I can run the examples successfully. But there is no source code for it.

Could anyone please advise how to start OpenGL application development on i.MX6 linux?

Thanks!

0 件の賞賛
返信
2 返答(返信)

2,931件の閲覧回数
art
NXP Employee
NXP Employee

Please refer to the attached document.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

2,931件の閲覧回数
frankchenmh
Contributor III

Hi Artur,

Thanks for your help. This document doesn't tell me how to setup OpenGL development environment on i.MX6 but it may still useful for me. Thanks!

0 件の賞賛
返信