OpenGL ES Benchmark Score

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

OpenGL ES Benchmark Score

Jump to solution
4,002 Views
wei-fonglin
Contributor II

Hi All,

I am working Yocto(L3.10.53_1.1.0) on i.MX6Q.

I execute glmark2-es2 and get score 53.

The questions are

1. Is this score high or low?

2. Because we don't have SABRESD. Could freescale provide the score of SABRESD for we reference?

Thanks,

Frank

Below is the log.

$ glmark2-es2 -s 1920x1080

=======================================================

    glmark2 2014.03

=======================================================

    OpenGL Information

    GL_VENDOR:     Vivante Corporation

    GL_RENDERER:   Vivante GC2000

    GL_VERSION:    OpenGL ES 3.0 V5.0.11.p4.25762

=======================================================

[build] use-vbo=false: FPS: 82 FrameTime: 12.195 ms

[build] use-vbo=true: FPS: 85 FrameTime: 11.765 ms

[texture] texture-filter=nearest: FPS: 68 FrameTime: 14.706 ms

[texture] texture-filter=linear: FPS: 67 FrameTime: 14.925 ms

[texture] texture-filter=mipmap: FPS: 65 FrameTime: 15.385 ms

[shading] shading=gouraud: FPS: 73 FrameTime: 13.699 ms

[shading] shading=blinn-phong-inf: FPS: 72 FrameTime: 13.889 ms

[shading] shading=phong: FPS: 72 FrameTime: 13.889 ms

[shading] shading=cel: FPS: 71 FrameTime: 14.085 ms

[bump] bump-render=high-poly: FPS: 76 FrameTime: 13.158 ms

[bump] bump-render=normals: FPS: 81 FrameTime: 12.346 ms

[bump] bump-render=height: FPS: 80 FrameTime: 12.500 ms

[effect2d] kernel=0,1,0;1,-4,1;0,1,0;: FPS: 35 FrameTime: 28.571 ms

[effect2d] kernel=1,1,1,1,1;1,1,1,1,1;1,1,1,1,1;: FPS: 21 FrameTime: 47.619 ms

[pulsar] light=false:quads=5:texture=false: FPS: 52 FrameTime: 19.231 ms

[desktop] blur-radius=5:effect=blur:passes=1:separable=true:windows=4: FPS: 12 FrameTime: 83.333 ms

[desktop] effect=shadow:windows=4: FPS: 31 FrameTime: 32.258 ms

[buffer] columns=200:interleave=false:update-dispersion=0.9:update-fraction=0.5:update-method=map: FPS: 34 FrameTime: 29.412 ms

[buffer] columns=200:interleave=false:update-dispersion=0.9:update-fraction=0.5:update-method=subdata: FPS: 34 FrameTime: 29.412 ms

[buffer] columns=200:interleave=true:update-dispersion=0.9:update-fraction=0.5:update-method=map: FPS: 45 FrameTime: 22.222 ms

[ideas] speed=duration: FPS: 24 FrameTime: 41.667 ms

[jellyfish] <default>: FPS: 44 FrameTime: 22.727 ms

[terrain] <default>: FPS: 0 FrameTime: inf ms

[shadow] <default>: FPS: 33 FrameTime: 30.303 ms

[refract] <default>: FPS: 9 FrameTime: 111.111 ms

[conditionals] fragment-steps=0:vertex-steps=0: FPS: 67 FrameTime: 14.925 ms

[conditionals] fragment-steps=5:vertex-steps=0: FPS: 61 FrameTime: 16.393 ms

[conditionals] fragment-steps=0:vertex-steps=5: FPS: 67 FrameTime: 14.925 ms

[function] fragment-complexity=low:fragment-steps=5: FPS: 66 FrameTime: 15.152 ms

[function] fragment-complexity=medium:fragment-steps=5: FPS: 44 FrameTime: 22.727 ms

[loop] fragment-loop=false:fragment-steps=5:vertex-steps=5: FPS: 66 FrameTime: 15.152 ms

[loop] fragment-steps=5:fragment-uniform=false:vertex-steps=5: FPS: 66 FrameTime: 15.152 ms

[loop] fragment-steps=5:fragment-uniform=true:vertex-steps=5: FPS: 64 FrameTime: 15.625 ms

=======================================================

                                  glmark2 Score: 53

=======================================================

Labels (4)
Tags (3)
0 Kudos
Reply
1 Solution
3,005 Views
jamesbone
NXP TechSupport
NXP TechSupport


Sorry, but the information you are requesting is treated as confidential info at this time and requires a signed NDA (Non-Disclosure Agreement). Naturally, we cannot discuss this with you in public anyway, this requires to be handled as a Service Request (SR). Be aware that to give you remote support through a SR, we will still need the confirmation of a Freescale employee that the NDA is in place. If you want to go this route, the next steps will be: If you have already signed a NDA agreement for this product, please contact the person who assisted you or create a SR and name us a Freescale person that can confirm this. If you have not signed an agreement, please contact your local Freescale Distributor Salesperson or FAE for assistance. For a listing of our distributors, refer to: http://www.freescale.com/webapp/sps/site/overview.jsp?code=DISTRIBUTORS

Have a great day,
Jaime

-------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
3,006 Views
jamesbone
NXP TechSupport
NXP TechSupport


Sorry, but the information you are requesting is treated as confidential info at this time and requires a signed NDA (Non-Disclosure Agreement). Naturally, we cannot discuss this with you in public anyway, this requires to be handled as a Service Request (SR). Be aware that to give you remote support through a SR, we will still need the confirmation of a Freescale employee that the NDA is in place. If you want to go this route, the next steps will be: If you have already signed a NDA agreement for this product, please contact the person who assisted you or create a SR and name us a Freescale person that can confirm this. If you have not signed an agreement, please contact your local Freescale Distributor Salesperson or FAE for assistance. For a listing of our distributors, refer to: http://www.freescale.com/webapp/sps/site/overview.jsp?code=DISTRIBUTORS

Have a great day,
Jaime

-------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-------------------------------------------------------------------------------

0 Kudos
Reply