OpenCV + Hardware Accelator

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

OpenCV + Hardware Accelator

1,728 次查看
byunggukchoi
Contributor II

I'm capturing images from a web camera connected to IMX6Q Sabre Auto.

The resolution of the web camera is 640x480 @ 30fps.

But the frame rate captured with "OpenCV+Python" is about 16 fps.

In order to increse performance, I want to use Hardware Accelator of IMX6Q.

By the way, I don't know how to enable hardware accelator and use OpenCV using hardware accelator.

Let me know the methods above.

Thanks in advance.

标签 (4)
1 回复

1,319 次查看
igorpadykov
NXP Employee
NXP Employee

Hi ByungGuk

please look on

Setting Up OpenCV in i.MX6 Based Boards 

Starting with OpenCV on i.MX6 processors 

about i.MX6 opencv 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------