OpenCV + Hardware Accelator

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

OpenCV + Hardware Accelator

1,725件の閲覧回数
byunggukchoi
Contributor II

I'm capturing images from a web camera connected to IMX6Q Sabre Auto.

The resolution of the web camera is 640x480 @ 30fps.

But the frame rate captured with "OpenCV+Python" is about 16 fps.

In order to increse performance, I want to use Hardware Accelator of IMX6Q.

By the way, I don't know how to enable hardware accelator and use OpenCV using hardware accelator.

Let me know the methods above.

Thanks in advance.

ラベル(4)
1 返信

1,316件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi ByungGuk

please look on

Setting Up OpenCV in i.MX6 Based Boards 

Starting with OpenCV on i.MX6 processors 

about i.MX6 opencv 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------