OpenCL not working with OpenCV on i.MX8M platform

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

OpenCL not working with OpenCV on i.MX8M platform

3,298 次查看
jrestifo
Contributor I
I am using an i.MX8M based platform with Vivante GC7000Lite GPU. (DART-MX8M from Variscite) I am trying to run OpenCV example code which is OpenCL accelerated but I am not getting what I expected, and wonder if there is some piece of info I am missing. For instance, if I try the opencv_test_optflow:
$ /usr/bin/opencv_test_optflow
[ WARN:0] Using world accessible cache directory. This may be not secure: /var/tmp/
[ INFO:0] Successfully initialized OpenCL cache directory: /var/tmp/opencv/3.4.0/opencl_cache/
[ INFO:0] Preparing OpenCL cache configuration for context: 32-bit--Vivante_Corporation--Vivante_OpenCL_Device_GC7000L_6214_0000--OpenCL_1_2_V6_2_4_p1_150331
OpenCL error CL_INVALID_WORK_GROUP_SIZE (-54) during call: clEnqueueNDRangeKernel('sobel3', dims=2, globalsize=592x400x1, localsize=16x16x1) sync=false
OpenCL error CL_INVALID_WORK_GROUP_SIZE (-54) during call: clEnqueueNDRangeKernel('maxEigenVal', dims=1, globalsize=4096x1x1, localsize=1024x1x1) sync=false
OpenCL error CL_INVALID_WORK_GROUP_SIZE (-54) during call: clEnqueueNDRangeKernel('pyrDown', dims=2, globalsize=768x97x1, localsize=256x1x1) sync=false
OpenCL error CL_INVALID_WORK_GROUP_SIZE (-54) during call: clEnqueueNDRangeKernel('pyrDown', dims=2, globalsize=768x97x1, localsize=256x1x1) sync=false
OpenCL error CL_INVALID_WORK_GROUP_SIZE (-54) during call: clEnqueueNDRangeKernel('pyrDown', dims=2, globalsize=512x49x1, localsize=256x1x1) sync=false
OpenCL error CL_INVALID_WORK_GROUP_SIZE (-54) during call: clEnqueueNDRangeKernel('pyrDown', dims=2, globalsize=512x49x1, localsize=256x1x1) sync=false
OpenCL error CL_INVALID_WORK_GROUP_SIZE (-54) during call: clEnqueueNDRangeKernel('pyrDown', dims=2, globalsize=256x25x1, localsize=256x1x1) sync=false
OpenCL error CL_INVALID_WORK_GROUP_SIZE (-54) during call: clEnqueueNDRangeKernel('pyrDown', dims=2, globalsize=256x25x1, localsize=256x1x1) sync=false
OpenCL error CL_INVALID_WORK_GROUP_SIZE (-54) during call: clEnqueueNDRangeKernel('pyrDown', dims=2, globalsize=768x97x1, localsize=256x1x1) sync=false
OpenCL error CL_INVALID_WORK_GROUP_SIZE (-54) during call: clEnqueueNDRangeKernel('pyrDown', dims=2, globalsize=768x97x1, localsize=256x1x1) sync=false
OpenCL error CL_INVALID_WORK_GROUP_SIZE (-54) during call: clEnqueueNDRangeKernel('pyrDown', dims=2, globalsize=512x49x1, localsize=256x1x1) sync=false
OpenCL error CL_INVALID_WORK_GROUP_SIZE (-54) during call: clEnqueueNDRangeKernel('pyrDown', dims=2, globalsize=512x49x1, localsize=256x1x1) sync=false
OpenCL error CL_INVALID_WORK_GROUP_SIZE (-54) during call: clEnqueueNDRangeKernel('pyrDown', dims=2, globalsize=256x25x1, localsize=256x1x1) sync=false
OpenCL error CL_INVALID_WORK_GROUP_SIZE (-54) during call: clEnqueueNDRangeKernel('pyrDown', dims=2, globalsize=256x25x1, localsize=256x1x1) sync=false
/usr/src/debug/opencv/3.4+gitAUTOINC+6d4f66472e_81ca8dab86_a62e20676a_34e4206aef_fccf7cd6a4-r0/contrib/modules/optflow/test/test_OF_accuracy.cpp:236: Failure
Expected: (calcRMSE(GT, flow)) <= (target_RMSE), actual: 0.5805 vs 0.55
[  FAILED  ] DenseOpticalFlow_PCAFlow.ReferenceAccuracy (65669 ms)
[----------] 1 test from DenseOpticalFlow_PCAFlow (65669 ms total)

What I do not understand is why CL_INVALID_WORK_GROUP_SIZE is returned. The localsize divides evenly into global size. It is less than global size. It is less than 1024 (max work group size). Why does it fail? If I pass NULL as localsize to clEnqueueNDRangeKernel it works, but this is not a general solution since I would need to hand modify all kernels which rely on a known localsize. It seems to me a potential bug in the underlying platform, either in the GPU itself or perhaps the BSP. However, the libVivanteOpenCL appears to be closed source so I cannot really investigate further. Please advise, thank you!
0 项奖励
回复
4 回复数

2,194 次查看
ChristianPrather
Contributor II

Has there been any progress on this?

0 项奖励
回复

2,829 次查看
1019599657
Contributor III

hi, can opencv use opencl in imx8 directly? Do you compile the source code?

0 项奖励
回复

2,829 次查看
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hi Jordan,

Error -54 is CL_INVALID_WORK_GROUP_SIZE - values in your "globalWorkSize" array are not divisible with values in your "localWorkSize" array, and that's it (remember that global work size is really total number of threads along each dimension, and not the size of the "block" of threads along corresponding dimension).

Regards

0 项奖励
回复

1,989 次查看
ChristianPrather
Contributor II

Hi can you elaborate on this please? As this is a consistent problem that I and others have seen, some additional advice would be greatly appreciated. 

Thank you

0 项奖励
回复