Program and run XiP with IMXRT1010-EVK

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Program and run XiP with IMXRT1010-EVK

Jump to solution
1,798 Views
threeboystech
Contributor II

Can someone share a link to the application note or other documentation on how to program the flash on the IMXRT1010-EVK development board.

I have working code running fine when linked to RAM, but I cannot seem to get anything to program or run from flash XiP.

Thanks

 

Labels (1)
0 Kudos
Reply
1 Solution
1,775 Views
Ramon_Vega
NXP TechSupport
NXP TechSupport

Dear @threeboystech 

You can program the flash on the IMXRT1010-EVK by using the Flashloader to program a bootable image into the external memory device either by using Open SDA or MfgTool.

You can find more information on how to do this in these application notes.

AN12108: How to Enable Boot from QSPI Flash – Application Note (nxp.com)

AN12238: i.MX RT Flashloader Use Case – Application Note (nxp.com)

Getting Started with i.MX RT1010 Evaluation Kit | NXP Semiconductors

External memory interfaces for the RT1010:

  • SPI NOR FLASH
  • Single/Dual channel Quad SPI FLASH with XIP support and on-the-fly decryption
  • Octal flash

I hope this information helps!.

Kind Regards.

-Ramon.

 

View solution in original post

0 Kudos
Reply
1 Reply
1,776 Views
Ramon_Vega
NXP TechSupport
NXP TechSupport

Dear @threeboystech 

You can program the flash on the IMXRT1010-EVK by using the Flashloader to program a bootable image into the external memory device either by using Open SDA or MfgTool.

You can find more information on how to do this in these application notes.

AN12108: How to Enable Boot from QSPI Flash – Application Note (nxp.com)

AN12238: i.MX RT Flashloader Use Case – Application Note (nxp.com)

Getting Started with i.MX RT1010 Evaluation Kit | NXP Semiconductors

External memory interfaces for the RT1010:

  • SPI NOR FLASH
  • Single/Dual channel Quad SPI FLASH with XIP support and on-the-fly decryption
  • Octal flash

I hope this information helps!.

Kind Regards.

-Ramon.

 

0 Kudos
Reply