On IMX8mp linux, how to enable SDMA for UART0 ?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

On IMX8mp linux, how to enable SDMA for UART0 ?

3,431件の閲覧回数
mahesh_hns
Contributor II

I was trying to enable DMA for UART0 (SDMA) on imx8mp linux 5.4.70.

When I built linux kernel with CONFIG_IMX_SDMA=y, I get this error during boot

 

[[ 0.712424] imx-sdma 30bd0000.dma-controller: Direct firmware load for imx/sdma/sdma-imx7d.bin failed with error -2
[ 0.712437] imx-sdma 30bd0000.dma-controller: Falling back to sysfs fallback for: imx/sdma/sdma-imx7d.bin
[ 0.713761] mxs-dma 33000000.dma-apbh: initialized

The firmware mx/sdma/sdma-imx7d.bin was indeed present at the location mentioned there. I wonder why I still got the error. 

So, how do I enable SDMA for UART0? And if once it is enabled, how do I know that SDMA has been enabled? Any sample logs? Any sysfs entries w.r.t sdma?

 

 

 

 

 

0 件の賞賛
返信
6 返答(返信)

3,367件の閲覧回数
mahesh_hns
Contributor II

Thanks. Is there any other way of checking if DMA is enabled? reading register values through devmem2?

0 件の賞賛
返信

3,345件の閲覧回数
AldoG
NXP TechSupport
NXP TechSupport

Hello,

yes, if you want to double check if dma is enabled for UART, you may read UARTx_UCRx registers, please refer to the i.MX8MP reference manual page 7341.

Best regards,
Aldo.

0 件の賞賛
返信

3,417件の閲覧回数
mahesh_hns
Contributor II

Some other threads mentioned it was due to the RFS not initialized by the the time the driver comes up, and hence the error. The suggested workaround was to build the driver as a module CONFIG_IMX_SDMA=m and load it early in the sequence. I saw that it was not automatically loading anyway. When I manually loaded the imx-sdma.ko file (kept in /lib/modules/kernel-<>/drivers/dma/) it loaded fine with the message 

[ 2179.476286] imx-sdma 30bd0000.dma-controller: loaded firmware 4.5

Even then I wasn't sure if the UART0 uses DMA at that point (as it is past the UART initialization). Guess I have to force reset UART which forces it to use DMA?

Any cleaner solution? Is it possible to CONFIG_IMX_SDMA=y and compile the firmware also in to the kernel image (with no RFS dependency) ?

0 件の賞賛
返信

3,390件の閲覧回数
mahesh_hns
Contributor II

Update: I pre-compiled the imx-sdma7.bin (from yocto generated RFS) using 

CONFIG_EXTRA_FIRMWARE="sdma-imx7d.bin"
CONFIG_EXTRA_FIRMWARE_DIR="lib/firmware"

And the boot messages have these

[ 0.713318] imx-sdma 30bd0000.dma-controller: loaded firmware 4.5

..........

[ 0.721005] Serial: 8250/16550 driver, 4 ports, IRQ sharing enabled
[ 0.722796] 30860000.serial: ttymxc0 at MMIO 0x30860000 (irq = 25, base_baud = 1500000) is a IMX
[ 0.723239] 30880000.serial: ttymxc2 at MMIO 0x30880000 (irq = 26, base_baud = 5000000) is a IMX
[ 0.723600] 30890000.serial: ttymxc1 at MMIO 0x30890000 (irq = 27, base_baud = 1500000) is a IMX
[ 1.694646] printk: console [ttymxc1] enabled

It looks like SDMA has firmware has been loaded successfully, but I don't see any other message on that. I am not sure if UART0 (ttymxc0) is using SDMA or not. Is there any way to find that?

The UART1 device tree have the following (entries in imx8mp.dtsi)

uart1 {

dmas = <&sdma1 22 4 0>, <&sdma1 23 4 0>;
dma-names = "rx", "tx";

..

}

How do I verify if the SDMA is enabled for ttymxc0 ? Any sysfs status checks?

0 件の賞賛
返信

1,444件の閲覧回数
gigli_korg
Contributor II
Hello mahesh_hns,

question: does the file "sdma-imx7d.bin" satisfy the GPL requirement?

Stefano
0 件の賞賛
返信

3,385件の閲覧回数
AldoG
NXP TechSupport
NXP TechSupport

Hello.

All you have done looks correct, regarding double checking if SDMA is enabled, then you may add some debug logs to the UART driver.

In UART driver, function dma_request_slave_channel() in imx_uart_dma_init() will return true when SDMA firmware is not loaded. You may add some log in UART driver to check when DMA is initialized.

Best regards,
Aldo.

0 件の賞賛
返信