OV5642 camera sensor clock.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

OV5642 camera sensor clock.

Jump to solution
5,838 Views
johnturnur
Contributor III

Hello AlI,

In our application we need to record live video using CSI 20 bit paralleled interface and rotate this video in 90 degree. We are using ov5642  as 20bit camera sensor. We are able to capture video and re sized and rotate it. While in preview mode it flickers display.

We are using platform SDK 1.1 code not V4l2 driver.

Is it problem of 0v5642 camera sensor or IPU display?

How we can set the ov5642 camera clock? How we can set frame per second (FPS) in ov5642 camera sensor.

Please help me to get this issue resolved.

Thanks,

J

Labels (4)
0 Kudos
Reply
1 Solution
4,593 Views
weidong_sun
NXP TechSupport
NXP TechSupport

Hi,John,

     Those settings are in ov5642.c :

static struct reg_value ov5642_setting_30fps_720P_1280_720[] = {

{0x3103, 0x93, 0, 0}, {0x3008, 0x82, 0, 0}, {0x3017, 0x7f, 0, 0},

{0x3018, 0xfc, 0, 0}, {0x3810, 0xc2, 0, 0}, {0x3615, 0xf0, 0, 0},

{0x3000, 0x00, 0, 0}, {0x3001, 0x00, 0, 0}, {0x3002, 0x00, 0, 0},

{0x3003, 0x00, 0, 0}, {0x3004, 0xff, 0, 0}, {0x3030, 0x2b, 0, 0},

{0x3011, 0x08, 0, 0}, {0x3010, 0x10, 0, 0}, {0x3604, 0x60, 0, 0},

{0x3622, 0x60, 0, 0}, {0x3621, 0x09, 0, 0}, {0x3709, 0x00, 0, 0},

{0x4000, 0x21, 0, 0}, {0x401d, 0x22, 0, 0}, {0x3600, 0x54, 0, 0},

{0x3605, 0x04, 0, 0}, {0x3606, 0x3f, 0, 0}, {0x3c01, 0x80, 0, 0},

{0x300d, 0x22, 0, 0}, {0x3623, 0x22, 0, 0}, {0x5000, 0x4f, 0, 0},

{0x5020, 0x04, 0, 0}, {0x5181, 0x79, 0, 0}, {0x5182, 0x00, 0, 0},

{0x5185, 0x22, 0, 0}, {0x5197, 0x01, 0, 0}, {0x5500, 0x0a, 0, 0},

{0x5504, 0x00, 0, 0}, {0x5505, 0x7f, 0, 0}, {0x5080, 0x08, 0, 0},

{0x300e, 0x18, 0, 0}, {0x4610, 0x00, 0, 0}, {0x471d, 0x05, 0, 0},

{0x4708, 0x06, 0, 0}, {0x370c, 0xa0, 0, 0}, {0x3808, 0x0a, 0, 0},

{0x3809, 0x20, 0, 0}, {0x380a, 0x07, 0, 0}, {0x380b, 0x98, 0, 0},

{0x380c, 0x0c, 0, 0}, {0x380d, 0x80, 0, 0}, {0x380e, 0x07, 0, 0},

{0x380f, 0xd0, 0, 0}, {0x5687, 0x94, 0, 0}, {0x501f, 0x00, 0, 0},

{0x5000, 0x4f, 0, 0}, {0x5001, 0xcf, 0, 0}, {0x4300, 0x30, 0, 0},

{0x4300, 0x30, 0, 0}, {0x460b, 0x35, 0, 0}, {0x471d, 0x00, 0, 0},

{0x3002, 0x0c, 0, 0}, {0x3002, 0x00, 0, 0}, {0x4713, 0x03, 0, 0},

{0x471c, 0x50, 0, 0}, {0x4721, 0x02, 0, 0}, {0x4402, 0x90, 0, 0},

{0x460c, 0x22, 0, 0}, {0x3815, 0x44, 0, 0}, {0x3503, 0x07, 0, 0},

{0x3501, 0x73, 0, 0}, {0x3502, 0x80, 0, 0}, {0x350b, 0x00, 0, 0},

{0x3818, 0xc8, 0, 0}, {0x3801, 0x88, 0, 0}, {0x3824, 0x11, 0, 0},

{0x3a00, 0x78, 0, 0}, {0x3a1a, 0x04, 0, 0}, {0x3a13, 0x30, 0, 0},

{0x3a18, 0x00, 0, 0}, {0x3a19, 0x7c, 0, 0}, {0x3a08, 0x12, 0, 0},

{0x3a09, 0xc0, 0, 0}, {0x3a0a, 0x0f, 0, 0}, {0x3a0b, 0xa0, 0, 0},

{0x350c, 0x07, 0, 0}, {0x350d, 0xd0, 0, 0}, {0x3a0d, 0x08, 0, 0},

{0x3a0e, 0x06, 0, 0}, {0x3500, 0x00, 0, 0}, {0x3501, 0x00, 0, 0},

{0x3502, 0x00, 0, 0}, {0x350a, 0x00, 0, 0}, {0x350b, 0x00, 0, 0},

{0x3503, 0x00, 0, 0}, {0x3a0f, 0x3c, 0, 0}, {0x3a10, 0x32, 0, 0},

{0x3a1b, 0x3c, 0, 0}, {0x3a1e, 0x32, 0, 0}, {0x3a11, 0x80, 0, 0},

{0x3a1f, 0x20, 0, 0}, {0x3030, 0x2b, 0, 0}, {0x3a02, 0x00, 0, 0},

{0x3a03, 0x7d, 0, 0}, {0x3a04, 0x00, 0, 0}, {0x3a14, 0x00, 0, 0},

{0x3a15, 0x7d, 0, 0}, {0x3a16, 0x00, 0, 0}, {0x3a00, 0x78, 0, 0},

{0x3a08, 0x09, 0, 0}, {0x3a09, 0x60, 0, 0}, {0x3a0a, 0x07, 0, 0},

{0x3a0b, 0xd0, 0, 0}, {0x3a0d, 0x10, 0, 0}, {0x3a0e, 0x0d, 0, 0},

{0x4407, 0x04, 0, 0}, {0x5193, 0x70, 0, 0}, {0x589b, 0x00, 0, 0},

{0x589a, 0xc0, 0, 0}, {0x401e, 0x20, 0, 0}, {0x4001, 0x42, 0, 0},

{0x401c, 0x06, 0, 0}, {0x3825, 0xac, 0, 0}, {0x3827, 0x0c, 0, 0},

{0x528a, 0x01, 0, 0}, {0x528b, 0x04, 0, 0}, {0x528c, 0x08, 0, 0},

{0x528d, 0x10, 0, 0}, {0x528e, 0x20, 0, 0}, {0x528f, 0x28, 0, 0},

{0x5290, 0x30, 0, 0}, {0x5292, 0x00, 0, 0}, {0x5293, 0x01, 0, 0},

{0x5294, 0x00, 0, 0}, {0x5295, 0x04, 0, 0}, {0x5296, 0x00, 0, 0},

{0x5297, 0x08, 0, 0}, {0x5298, 0x00, 0, 0}, {0x5299, 0x10, 0, 0},

{0x529a, 0x00, 0, 0}, {0x529b, 0x20, 0, 0}, {0x529c, 0x00, 0, 0},

{0x529d, 0x28, 0, 0}, {0x529e, 0x00, 0, 0}, {0x529f, 0x30, 0, 0},

{0x5282, 0x00, 0, 0}, {0x5300, 0x00, 0, 0}, {0x5301, 0x20, 0, 0},

{0x5302, 0x00, 0, 0}, {0x5303, 0x7c, 0, 0}, {0x530c, 0x00, 0, 0},

{0x530d, 0x0c, 0, 0}, {0x530e, 0x20, 0, 0}, {0x530f, 0x80, 0, 0},

{0x5310, 0x20, 0, 0}, {0x5311, 0x80, 0, 0}, {0x5308, 0x20, 0, 0},

{0x5309, 0x40, 0, 0}, {0x5304, 0x00, 0, 0}, {0x5305, 0x30, 0, 0},

{0x5306, 0x00, 0, 0}, {0x5307, 0x80, 0, 0}, {0x5314, 0x08, 0, 0},

{0x5315, 0x20, 0, 0}, {0x5319, 0x30, 0, 0}, {0x5316, 0x10, 0, 0},

{0x5317, 0x00, 0, 0}, {0x5318, 0x02, 0, 0}, {0x5380, 0x01, 0, 0},

{0x5381, 0x00, 0, 0}, {0x5382, 0x00, 0, 0}, {0x5383, 0x4e, 0, 0},

{0x5384, 0x00, 0, 0}, {0x5385, 0x0f, 0, 0}, {0x5386, 0x00, 0, 0},

{0x5387, 0x00, 0, 0}, {0x5388, 0x01, 0, 0}, {0x5389, 0x15, 0, 0},

{0x538a, 0x00, 0, 0}, {0x538b, 0x31, 0, 0}, {0x538c, 0x00, 0, 0},

{0x538d, 0x00, 0, 0}, {0x538e, 0x00, 0, 0}, {0x538f, 0x0f, 0, 0},

{0x5390, 0x00, 0, 0}, {0x5391, 0xab, 0, 0}, {0x5392, 0x00, 0, 0},

{0x5393, 0xa2, 0, 0}, {0x5394, 0x08, 0, 0}, {0x5480, 0x14, 0, 0},

{0x5481, 0x21, 0, 0}, {0x5482, 0x36, 0, 0}, {0x5483, 0x57, 0, 0},

{0x5484, 0x65, 0, 0}, {0x5485, 0x71, 0, 0}, {0x5486, 0x7d, 0, 0},

{0x5487, 0x87, 0, 0}, {0x5488, 0x91, 0, 0}, {0x5489, 0x9a, 0, 0},

{0x548a, 0xaa, 0, 0}, {0x548b, 0xb8, 0, 0}, {0x548c, 0xcd, 0, 0},

{0x548d, 0xdd, 0, 0}, {0x548e, 0xea, 0, 0}, {0x548f, 0x1d, 0, 0},

{0x5490, 0x05, 0, 0}, {0x5491, 0x00, 0, 0}, {0x5492, 0x04, 0, 0},

{0x5493, 0x20, 0, 0}, {0x5494, 0x03, 0, 0}, {0x5495, 0x60, 0, 0},

{0x5496, 0x02, 0, 0}, {0x5497, 0xb8, 0, 0}, {0x5498, 0x02, 0, 0},

{0x5499, 0x86, 0, 0}, {0x549a, 0x02, 0, 0}, {0x549b, 0x5b, 0, 0},

{0x549c, 0x02, 0, 0}, {0x549d, 0x3b, 0, 0}, {0x549e, 0x02, 0, 0},

{0x549f, 0x1c, 0, 0}, {0x54a0, 0x02, 0, 0}, {0x54a1, 0x04, 0, 0},

{0x54a2, 0x01, 0, 0}, {0x54a3, 0xed, 0, 0}, {0x54a4, 0x01, 0, 0},

{0x54a5, 0xc5, 0, 0}, {0x54a6, 0x01, 0, 0}, {0x54a7, 0xa5, 0, 0},

{0x54a8, 0x01, 0, 0}, {0x54a9, 0x6c, 0, 0}, {0x54aa, 0x01, 0, 0},

{0x54ab, 0x41, 0, 0}, {0x54ac, 0x01, 0, 0}, {0x54ad, 0x20, 0, 0},

{0x54ae, 0x00, 0, 0}, {0x54af, 0x16, 0, 0}, {0x54b0, 0x01, 0, 0},

{0x54b1, 0x20, 0, 0}, {0x54b2, 0x00, 0, 0}, {0x54b3, 0x10, 0, 0},

{0x54b4, 0x00, 0, 0}, {0x54b5, 0xf0, 0, 0}, {0x54b6, 0x00, 0, 0},

{0x54b7, 0xdf, 0, 0}, {0x5402, 0x3f, 0, 0}, {0x5403, 0x00, 0, 0},

{0x3406, 0x00, 0, 0}, {0x5180, 0xff, 0, 0}, {0x5181, 0x52, 0, 0},

{0x5182, 0x11, 0, 0}, {0x5183, 0x14, 0, 0}, {0x5184, 0x25, 0, 0},

{0x5185, 0x24, 0, 0}, {0x5186, 0x06, 0, 0}, {0x5187, 0x08, 0, 0},

{0x5188, 0x08, 0, 0}, {0x5189, 0x7c, 0, 0}, {0x518a, 0x60, 0, 0},

{0x518b, 0xb2, 0, 0}, {0x518c, 0xb2, 0, 0}, {0x518d, 0x44, 0, 0},

{0x518e, 0x3d, 0, 0}, {0x518f, 0x58, 0, 0}, {0x5190, 0x46, 0, 0},

{0x5191, 0xf8, 0, 0}, {0x5192, 0x04, 0, 0}, {0x5193, 0x70, 0, 0},

{0x5194, 0xf0, 0, 0}, {0x5195, 0xf0, 0, 0}, {0x5196, 0x03, 0, 0},

{0x5197, 0x01, 0, 0}, {0x5198, 0x04, 0, 0}, {0x5199, 0x12, 0, 0},

{0x519a, 0x04, 0, 0}, {0x519b, 0x00, 0, 0}, {0x519c, 0x06, 0, 0},

{0x519d, 0x82, 0, 0}, {0x519e, 0x00, 0, 0}, {0x5025, 0x80, 0, 0},

{0x3a0f, 0x38, 0, 0}, {0x3a10, 0x30, 0, 0}, {0x3a1b, 0x3a, 0, 0},

{0x3a1e, 0x2e, 0, 0}, {0x3a11, 0x60, 0, 0}, {0x3a1f, 0x10, 0, 0},

{0x5688, 0xa6, 0, 0}, {0x5689, 0x6a, 0, 0}, {0x568a, 0xea, 0, 0},

{0x568b, 0xae, 0, 0}, {0x568c, 0xa6, 0, 0}, {0x568d, 0x6a, 0, 0},

{0x568e, 0x62, 0, 0}, {0x568f, 0x26, 0, 0}, {0x5583, 0x40, 0, 0},

{0x5584, 0x40, 0, 0}, {0x5580, 0x02, 0, 0}, {0x5000, 0xcf, 0, 0},

{0x5800, 0x27, 0, 0}, {0x5801, 0x19, 0, 0}, {0x5802, 0x12, 0, 0},

{0x5803, 0x0f, 0, 0}, {0x5804, 0x10, 0, 0}, {0x5805, 0x15, 0, 0},

{0x5806, 0x1e, 0, 0}, {0x5807, 0x2f, 0, 0}, {0x5808, 0x15, 0, 0},

{0x5809, 0x0d, 0, 0}, {0x580a, 0x0a, 0, 0}, {0x580b, 0x09, 0, 0},

{0x580c, 0x0a, 0, 0}, {0x580d, 0x0c, 0, 0}, {0x580e, 0x12, 0, 0},

{0x580f, 0x19, 0, 0}, {0x5810, 0x0b, 0, 0}, {0x5811, 0x07, 0, 0},

{0x5812, 0x04, 0, 0}, {0x5813, 0x03, 0, 0}, {0x5814, 0x03, 0, 0},

{0x5815, 0x06, 0, 0}, {0x5816, 0x0a, 0, 0}, {0x5817, 0x0f, 0, 0},

{0x5818, 0x0a, 0, 0}, {0x5819, 0x05, 0, 0}, {0x581a, 0x01, 0, 0},

{0x581b, 0x00, 0, 0}, {0x581c, 0x00, 0, 0}, {0x581d, 0x03, 0, 0},

{0x581e, 0x08, 0, 0}, {0x581f, 0x0c, 0, 0}, {0x5820, 0x0a, 0, 0},

{0x5821, 0x05, 0, 0}, {0x5822, 0x01, 0, 0}, {0x5823, 0x00, 0, 0},

{0x5824, 0x00, 0, 0}, {0x5825, 0x03, 0, 0}, {0x5826, 0x08, 0, 0},

{0x5827, 0x0c, 0, 0}, {0x5828, 0x0e, 0, 0}, {0x5829, 0x08, 0, 0},

{0x582a, 0x06, 0, 0}, {0x582b, 0x04, 0, 0}, {0x582c, 0x05, 0, 0},

{0x582d, 0x07, 0, 0}, {0x582e, 0x0b, 0, 0}, {0x582f, 0x12, 0, 0},

{0x5830, 0x18, 0, 0}, {0x5831, 0x10, 0, 0}, {0x5832, 0x0c, 0, 0},

{0x5833, 0x0a, 0, 0}, {0x5834, 0x0b, 0, 0}, {0x5835, 0x0e, 0, 0},

{0x5836, 0x15, 0, 0}, {0x5837, 0x19, 0, 0}, {0x5838, 0x32, 0, 0},

{0x5839, 0x1f, 0, 0}, {0x583a, 0x18, 0, 0}, {0x583b, 0x16, 0, 0},

{0x583c, 0x17, 0, 0}, {0x583d, 0x1e, 0, 0}, {0x583e, 0x26, 0, 0},

{0x583f, 0x53, 0, 0}, {0x5840, 0x10, 0, 0}, {0x5841, 0x0f, 0, 0},

{0x5842, 0x0d, 0, 0}, {0x5843, 0x0c, 0, 0}, {0x5844, 0x0e, 0, 0},

{0x5845, 0x09, 0, 0}, {0x5846, 0x11, 0, 0}, {0x5847, 0x10, 0, 0},

{0x5848, 0x10, 0, 0}, {0x5849, 0x10, 0, 0}, {0x584a, 0x10, 0, 0},

{0x584b, 0x0e, 0, 0}, {0x584c, 0x10, 0, 0}, {0x584d, 0x10, 0, 0},

{0x584e, 0x11, 0, 0}, {0x584f, 0x10, 0, 0}, {0x5850, 0x0f, 0, 0},

{0x5851, 0x0c, 0, 0}, {0x5852, 0x0f, 0, 0}, {0x5853, 0x10, 0, 0},

{0x5854, 0x10, 0, 0}, {0x5855, 0x0f, 0, 0}, {0x5856, 0x0e, 0, 0},

{0x5857, 0x0b, 0, 0}, {0x5858, 0x10, 0, 0}, {0x5859, 0x0d, 0, 0},

{0x585a, 0x0d, 0, 0}, {0x585b, 0x0c, 0, 0}, {0x585c, 0x0c, 0, 0},

{0x585d, 0x0c, 0, 0}, {0x585e, 0x0b, 0, 0}, {0x585f, 0x0c, 0, 0},

{0x5860, 0x0c, 0, 0}, {0x5861, 0x0c, 0, 0}, {0x5862, 0x0d, 0, 0},

{0x5863, 0x08, 0, 0}, {0x5864, 0x11, 0, 0}, {0x5865, 0x18, 0, 0},

{0x5866, 0x18, 0, 0}, {0x5867, 0x19, 0, 0}, {0x5868, 0x17, 0, 0},

{0x5869, 0x19, 0, 0}, {0x586a, 0x16, 0, 0}, {0x586b, 0x13, 0, 0},

{0x586c, 0x13, 0, 0}, {0x586d, 0x12, 0, 0}, {0x586e, 0x13, 0, 0},

{0x586f, 0x16, 0, 0}, {0x5870, 0x14, 0, 0}, {0x5871, 0x12, 0, 0},

{0x5872, 0x10, 0, 0}, {0x5873, 0x11, 0, 0}, {0x5874, 0x11, 0, 0},

{0x5875, 0x16, 0, 0}, {0x5876, 0x14, 0, 0}, {0x5877, 0x11, 0, 0},

{0x5878, 0x10, 0, 0}, {0x5879, 0x0f, 0, 0}, {0x587a, 0x10, 0, 0},

{0x587b, 0x14, 0, 0}, {0x587c, 0x13, 0, 0}, {0x587d, 0x12, 0, 0},

{0x587e, 0x11, 0, 0}, {0x587f, 0x11, 0, 0}, {0x5880, 0x12, 0, 0},

{0x5881, 0x15, 0, 0}, {0x5882, 0x14, 0, 0}, {0x5883, 0x15, 0, 0},

{0x5884, 0x15, 0, 0}, {0x5885, 0x15, 0, 0}, {0x5886, 0x13, 0, 0},

{0x5887, 0x17, 0, 0}, {0x3710, 0x10, 0, 0}, {0x3632, 0x51, 0, 0},

{0x3702, 0x10, 0, 0}, {0x3703, 0xb2, 0, 0}, {0x3704, 0x18, 0, 0},

{0x370b, 0x40, 0, 0}, {0x370d, 0x03, 0, 0}, {0x3631, 0x01, 0, 0},

{0x3632, 0x52, 0, 0}, {0x3606, 0x24, 0, 0}, {0x3620, 0x96, 0, 0},

{0x5785, 0x07, 0, 0}, {0x3a13, 0x30, 0, 0}, {0x3600, 0x52, 0, 0},

{0x3604, 0x48, 0, 0}, {0x3606, 0x1b, 0, 0}, {0x370d, 0x0b, 0, 0},

{0x370f, 0xc0, 0, 0}, {0x3709, 0x01, 0, 0}, {0x3823, 0x00, 0, 0},

{0x5007, 0x00, 0, 0}, {0x5009, 0x00, 0, 0}, {0x5011, 0x00, 0, 0},

{0x5013, 0x00, 0, 0}, {0x519e, 0x00, 0, 0}, {0x5086, 0x00, 0, 0},

{0x5087, 0x00, 0, 0}, {0x5088, 0x00, 0, 0}, {0x5089, 0x00, 0, 0},

{0x302b, 0x00, 0, 0}, {0x3503, 0x07, 0, 0}, {0x3011, 0x08, 0, 0},

{0x350c, 0x02, 0, 0}, {0x350d, 0xe4, 0, 0}, {0x3621, 0xc9, 0, 0},

{0x370a, 0x81, 0, 0}, {0x3803, 0x08, 0, 0}, {0x3804, 0x05, 0, 0},

{0x3805, 0x00, 0, 0}, {0x3806, 0x02, 0, 0}, {0x3807, 0xd0, 0, 0},

{0x3808, 0x05, 0, 0}, {0x3809, 0x00, 0, 0}, {0x380a, 0x02, 0, 0},

{0x380b, 0xd0, 0, 0}, {0x380c, 0x08, 0, 0}, {0x380d, 0x72, 0, 0},

{0x380e, 0x02, 0, 0}, {0x380f, 0xe4, 0, 0}, {0x3810, 0xc0, 0, 0},

{0x3818, 0xc9, 0, 0}, {0x381c, 0x10, 0, 0}, {0x381d, 0xa0, 0, 0},

{0x381e, 0x05, 0, 0}, {0x381f, 0xb0, 0, 0}, {0x3820, 0x00, 0, 0},

{0x3821, 0x00, 0, 0}, {0x3824, 0x11, 0, 0}, {0x3a08, 0x1b, 0, 0},

{0x3a09, 0xc0, 0, 0}, {0x3a0a, 0x17, 0, 0}, {0x3a0b, 0x20, 0, 0},

{0x3a0d, 0x02, 0, 0}, {0x3a0e, 0x01, 0, 0}, {0x401c, 0x04, 0, 0},

{0x5682, 0x05, 0, 0}, {0x5683, 0x00, 0, 0}, {0x5686, 0x02, 0, 0},

{0x5687, 0xcc, 0, 0}, {0x5001, 0x7f, 0, 0}, {0x589b, 0x06, 0, 0},

{0x589a, 0xc5, 0, 0}, {0x3503, 0x00, 0, 0}, {0x3010, 0x10, 0, 0},

{0x460c, 0x20, 0, 0}, {0x460b, 0x37, 0, 0}, {0x471c, 0xd0, 0, 0},

{0x471d, 0x05, 0, 0}, {0x3815, 0x01, 0, 0}, {0x3818, 0x00, 0x08, 0},

{0x501f, 0x00, 0, 0}, {0x4300, 0x30, 0, 0}, {0x3002, 0x1c, 0, 0},

{0x3819, 0x80, 0, 0}, {0x5002, 0xe0, 0, 0},

};

Weidong

View solution in original post

0 Kudos
Reply
7 Replies
4,593 Views
weidong_sun
NXP TechSupport
NXP TechSupport

Hello,John,

     I don't konw which CPU you are using. OV5642 needs 24MHz clock. For i.MX53 and i.MX6DQ, This 24MHz can be iomuxed via GPIO_0 pin.

     If you want image to rotate 90 degree, you don't need re-configure IPU display. In OV5642, there are several registers for image "Mirror or Flip" or "Mirror+flip". More details, you can look through OV5642 datasheet.

 

Regards,

Weidong

4,593 Views
johnturnur
Contributor III

Thanks sun for your quick reply.

I am using IMX6Q SDP platform board. IF i want to capture the video of 1024*768 @ 30 fps. will the 24 mhz be enough?

If i want to change the Clock what register of OV5642 needs to modify"?

thanks

j

0 Kudos
Reply
4,593 Views
weidong_sun
NXP TechSupport
NXP TechSupport

Hello,John,

      24MHz clock is a Main Clock(MCLK) for OV5642, OV5642's internal PLL and divider will convert it to other clock frequency that the module needs. This job will be done by OV5642 driver.

     It's no problem for 1024x768@30fs. I have ever tried 1280x720@30fs.

   

Regard,

Weidong

4,593 Views
johnturnur
Contributor III

Thanks for your quick reply.

Can you send me the register settings array of 0v5642 for your 1280x720@30fs? IT will be helpful for me to set that value as i am new to this.

Thanks in advance

J

0 Kudos
Reply
4,594 Views
weidong_sun
NXP TechSupport
NXP TechSupport

Hi,John,

     Those settings are in ov5642.c :

static struct reg_value ov5642_setting_30fps_720P_1280_720[] = {

{0x3103, 0x93, 0, 0}, {0x3008, 0x82, 0, 0}, {0x3017, 0x7f, 0, 0},

{0x3018, 0xfc, 0, 0}, {0x3810, 0xc2, 0, 0}, {0x3615, 0xf0, 0, 0},

{0x3000, 0x00, 0, 0}, {0x3001, 0x00, 0, 0}, {0x3002, 0x00, 0, 0},

{0x3003, 0x00, 0, 0}, {0x3004, 0xff, 0, 0}, {0x3030, 0x2b, 0, 0},

{0x3011, 0x08, 0, 0}, {0x3010, 0x10, 0, 0}, {0x3604, 0x60, 0, 0},

{0x3622, 0x60, 0, 0}, {0x3621, 0x09, 0, 0}, {0x3709, 0x00, 0, 0},

{0x4000, 0x21, 0, 0}, {0x401d, 0x22, 0, 0}, {0x3600, 0x54, 0, 0},

{0x3605, 0x04, 0, 0}, {0x3606, 0x3f, 0, 0}, {0x3c01, 0x80, 0, 0},

{0x300d, 0x22, 0, 0}, {0x3623, 0x22, 0, 0}, {0x5000, 0x4f, 0, 0},

{0x5020, 0x04, 0, 0}, {0x5181, 0x79, 0, 0}, {0x5182, 0x00, 0, 0},

{0x5185, 0x22, 0, 0}, {0x5197, 0x01, 0, 0}, {0x5500, 0x0a, 0, 0},

{0x5504, 0x00, 0, 0}, {0x5505, 0x7f, 0, 0}, {0x5080, 0x08, 0, 0},

{0x300e, 0x18, 0, 0}, {0x4610, 0x00, 0, 0}, {0x471d, 0x05, 0, 0},

{0x4708, 0x06, 0, 0}, {0x370c, 0xa0, 0, 0}, {0x3808, 0x0a, 0, 0},

{0x3809, 0x20, 0, 0}, {0x380a, 0x07, 0, 0}, {0x380b, 0x98, 0, 0},

{0x380c, 0x0c, 0, 0}, {0x380d, 0x80, 0, 0}, {0x380e, 0x07, 0, 0},

{0x380f, 0xd0, 0, 0}, {0x5687, 0x94, 0, 0}, {0x501f, 0x00, 0, 0},

{0x5000, 0x4f, 0, 0}, {0x5001, 0xcf, 0, 0}, {0x4300, 0x30, 0, 0},

{0x4300, 0x30, 0, 0}, {0x460b, 0x35, 0, 0}, {0x471d, 0x00, 0, 0},

{0x3002, 0x0c, 0, 0}, {0x3002, 0x00, 0, 0}, {0x4713, 0x03, 0, 0},

{0x471c, 0x50, 0, 0}, {0x4721, 0x02, 0, 0}, {0x4402, 0x90, 0, 0},

{0x460c, 0x22, 0, 0}, {0x3815, 0x44, 0, 0}, {0x3503, 0x07, 0, 0},

{0x3501, 0x73, 0, 0}, {0x3502, 0x80, 0, 0}, {0x350b, 0x00, 0, 0},

{0x3818, 0xc8, 0, 0}, {0x3801, 0x88, 0, 0}, {0x3824, 0x11, 0, 0},

{0x3a00, 0x78, 0, 0}, {0x3a1a, 0x04, 0, 0}, {0x3a13, 0x30, 0, 0},

{0x3a18, 0x00, 0, 0}, {0x3a19, 0x7c, 0, 0}, {0x3a08, 0x12, 0, 0},

{0x3a09, 0xc0, 0, 0}, {0x3a0a, 0x0f, 0, 0}, {0x3a0b, 0xa0, 0, 0},

{0x350c, 0x07, 0, 0}, {0x350d, 0xd0, 0, 0}, {0x3a0d, 0x08, 0, 0},

{0x3a0e, 0x06, 0, 0}, {0x3500, 0x00, 0, 0}, {0x3501, 0x00, 0, 0},

{0x3502, 0x00, 0, 0}, {0x350a, 0x00, 0, 0}, {0x350b, 0x00, 0, 0},

{0x3503, 0x00, 0, 0}, {0x3a0f, 0x3c, 0, 0}, {0x3a10, 0x32, 0, 0},

{0x3a1b, 0x3c, 0, 0}, {0x3a1e, 0x32, 0, 0}, {0x3a11, 0x80, 0, 0},

{0x3a1f, 0x20, 0, 0}, {0x3030, 0x2b, 0, 0}, {0x3a02, 0x00, 0, 0},

{0x3a03, 0x7d, 0, 0}, {0x3a04, 0x00, 0, 0}, {0x3a14, 0x00, 0, 0},

{0x3a15, 0x7d, 0, 0}, {0x3a16, 0x00, 0, 0}, {0x3a00, 0x78, 0, 0},

{0x3a08, 0x09, 0, 0}, {0x3a09, 0x60, 0, 0}, {0x3a0a, 0x07, 0, 0},

{0x3a0b, 0xd0, 0, 0}, {0x3a0d, 0x10, 0, 0}, {0x3a0e, 0x0d, 0, 0},

{0x4407, 0x04, 0, 0}, {0x5193, 0x70, 0, 0}, {0x589b, 0x00, 0, 0},

{0x589a, 0xc0, 0, 0}, {0x401e, 0x20, 0, 0}, {0x4001, 0x42, 0, 0},

{0x401c, 0x06, 0, 0}, {0x3825, 0xac, 0, 0}, {0x3827, 0x0c, 0, 0},

{0x528a, 0x01, 0, 0}, {0x528b, 0x04, 0, 0}, {0x528c, 0x08, 0, 0},

{0x528d, 0x10, 0, 0}, {0x528e, 0x20, 0, 0}, {0x528f, 0x28, 0, 0},

{0x5290, 0x30, 0, 0}, {0x5292, 0x00, 0, 0}, {0x5293, 0x01, 0, 0},

{0x5294, 0x00, 0, 0}, {0x5295, 0x04, 0, 0}, {0x5296, 0x00, 0, 0},

{0x5297, 0x08, 0, 0}, {0x5298, 0x00, 0, 0}, {0x5299, 0x10, 0, 0},

{0x529a, 0x00, 0, 0}, {0x529b, 0x20, 0, 0}, {0x529c, 0x00, 0, 0},

{0x529d, 0x28, 0, 0}, {0x529e, 0x00, 0, 0}, {0x529f, 0x30, 0, 0},

{0x5282, 0x00, 0, 0}, {0x5300, 0x00, 0, 0}, {0x5301, 0x20, 0, 0},

{0x5302, 0x00, 0, 0}, {0x5303, 0x7c, 0, 0}, {0x530c, 0x00, 0, 0},

{0x530d, 0x0c, 0, 0}, {0x530e, 0x20, 0, 0}, {0x530f, 0x80, 0, 0},

{0x5310, 0x20, 0, 0}, {0x5311, 0x80, 0, 0}, {0x5308, 0x20, 0, 0},

{0x5309, 0x40, 0, 0}, {0x5304, 0x00, 0, 0}, {0x5305, 0x30, 0, 0},

{0x5306, 0x00, 0, 0}, {0x5307, 0x80, 0, 0}, {0x5314, 0x08, 0, 0},

{0x5315, 0x20, 0, 0}, {0x5319, 0x30, 0, 0}, {0x5316, 0x10, 0, 0},

{0x5317, 0x00, 0, 0}, {0x5318, 0x02, 0, 0}, {0x5380, 0x01, 0, 0},

{0x5381, 0x00, 0, 0}, {0x5382, 0x00, 0, 0}, {0x5383, 0x4e, 0, 0},

{0x5384, 0x00, 0, 0}, {0x5385, 0x0f, 0, 0}, {0x5386, 0x00, 0, 0},

{0x5387, 0x00, 0, 0}, {0x5388, 0x01, 0, 0}, {0x5389, 0x15, 0, 0},

{0x538a, 0x00, 0, 0}, {0x538b, 0x31, 0, 0}, {0x538c, 0x00, 0, 0},

{0x538d, 0x00, 0, 0}, {0x538e, 0x00, 0, 0}, {0x538f, 0x0f, 0, 0},

{0x5390, 0x00, 0, 0}, {0x5391, 0xab, 0, 0}, {0x5392, 0x00, 0, 0},

{0x5393, 0xa2, 0, 0}, {0x5394, 0x08, 0, 0}, {0x5480, 0x14, 0, 0},

{0x5481, 0x21, 0, 0}, {0x5482, 0x36, 0, 0}, {0x5483, 0x57, 0, 0},

{0x5484, 0x65, 0, 0}, {0x5485, 0x71, 0, 0}, {0x5486, 0x7d, 0, 0},

{0x5487, 0x87, 0, 0}, {0x5488, 0x91, 0, 0}, {0x5489, 0x9a, 0, 0},

{0x548a, 0xaa, 0, 0}, {0x548b, 0xb8, 0, 0}, {0x548c, 0xcd, 0, 0},

{0x548d, 0xdd, 0, 0}, {0x548e, 0xea, 0, 0}, {0x548f, 0x1d, 0, 0},

{0x5490, 0x05, 0, 0}, {0x5491, 0x00, 0, 0}, {0x5492, 0x04, 0, 0},

{0x5493, 0x20, 0, 0}, {0x5494, 0x03, 0, 0}, {0x5495, 0x60, 0, 0},

{0x5496, 0x02, 0, 0}, {0x5497, 0xb8, 0, 0}, {0x5498, 0x02, 0, 0},

{0x5499, 0x86, 0, 0}, {0x549a, 0x02, 0, 0}, {0x549b, 0x5b, 0, 0},

{0x549c, 0x02, 0, 0}, {0x549d, 0x3b, 0, 0}, {0x549e, 0x02, 0, 0},

{0x549f, 0x1c, 0, 0}, {0x54a0, 0x02, 0, 0}, {0x54a1, 0x04, 0, 0},

{0x54a2, 0x01, 0, 0}, {0x54a3, 0xed, 0, 0}, {0x54a4, 0x01, 0, 0},

{0x54a5, 0xc5, 0, 0}, {0x54a6, 0x01, 0, 0}, {0x54a7, 0xa5, 0, 0},

{0x54a8, 0x01, 0, 0}, {0x54a9, 0x6c, 0, 0}, {0x54aa, 0x01, 0, 0},

{0x54ab, 0x41, 0, 0}, {0x54ac, 0x01, 0, 0}, {0x54ad, 0x20, 0, 0},

{0x54ae, 0x00, 0, 0}, {0x54af, 0x16, 0, 0}, {0x54b0, 0x01, 0, 0},

{0x54b1, 0x20, 0, 0}, {0x54b2, 0x00, 0, 0}, {0x54b3, 0x10, 0, 0},

{0x54b4, 0x00, 0, 0}, {0x54b5, 0xf0, 0, 0}, {0x54b6, 0x00, 0, 0},

{0x54b7, 0xdf, 0, 0}, {0x5402, 0x3f, 0, 0}, {0x5403, 0x00, 0, 0},

{0x3406, 0x00, 0, 0}, {0x5180, 0xff, 0, 0}, {0x5181, 0x52, 0, 0},

{0x5182, 0x11, 0, 0}, {0x5183, 0x14, 0, 0}, {0x5184, 0x25, 0, 0},

{0x5185, 0x24, 0, 0}, {0x5186, 0x06, 0, 0}, {0x5187, 0x08, 0, 0},

{0x5188, 0x08, 0, 0}, {0x5189, 0x7c, 0, 0}, {0x518a, 0x60, 0, 0},

{0x518b, 0xb2, 0, 0}, {0x518c, 0xb2, 0, 0}, {0x518d, 0x44, 0, 0},

{0x518e, 0x3d, 0, 0}, {0x518f, 0x58, 0, 0}, {0x5190, 0x46, 0, 0},

{0x5191, 0xf8, 0, 0}, {0x5192, 0x04, 0, 0}, {0x5193, 0x70, 0, 0},

{0x5194, 0xf0, 0, 0}, {0x5195, 0xf0, 0, 0}, {0x5196, 0x03, 0, 0},

{0x5197, 0x01, 0, 0}, {0x5198, 0x04, 0, 0}, {0x5199, 0x12, 0, 0},

{0x519a, 0x04, 0, 0}, {0x519b, 0x00, 0, 0}, {0x519c, 0x06, 0, 0},

{0x519d, 0x82, 0, 0}, {0x519e, 0x00, 0, 0}, {0x5025, 0x80, 0, 0},

{0x3a0f, 0x38, 0, 0}, {0x3a10, 0x30, 0, 0}, {0x3a1b, 0x3a, 0, 0},

{0x3a1e, 0x2e, 0, 0}, {0x3a11, 0x60, 0, 0}, {0x3a1f, 0x10, 0, 0},

{0x5688, 0xa6, 0, 0}, {0x5689, 0x6a, 0, 0}, {0x568a, 0xea, 0, 0},

{0x568b, 0xae, 0, 0}, {0x568c, 0xa6, 0, 0}, {0x568d, 0x6a, 0, 0},

{0x568e, 0x62, 0, 0}, {0x568f, 0x26, 0, 0}, {0x5583, 0x40, 0, 0},

{0x5584, 0x40, 0, 0}, {0x5580, 0x02, 0, 0}, {0x5000, 0xcf, 0, 0},

{0x5800, 0x27, 0, 0}, {0x5801, 0x19, 0, 0}, {0x5802, 0x12, 0, 0},

{0x5803, 0x0f, 0, 0}, {0x5804, 0x10, 0, 0}, {0x5805, 0x15, 0, 0},

{0x5806, 0x1e, 0, 0}, {0x5807, 0x2f, 0, 0}, {0x5808, 0x15, 0, 0},

{0x5809, 0x0d, 0, 0}, {0x580a, 0x0a, 0, 0}, {0x580b, 0x09, 0, 0},

{0x580c, 0x0a, 0, 0}, {0x580d, 0x0c, 0, 0}, {0x580e, 0x12, 0, 0},

{0x580f, 0x19, 0, 0}, {0x5810, 0x0b, 0, 0}, {0x5811, 0x07, 0, 0},

{0x5812, 0x04, 0, 0}, {0x5813, 0x03, 0, 0}, {0x5814, 0x03, 0, 0},

{0x5815, 0x06, 0, 0}, {0x5816, 0x0a, 0, 0}, {0x5817, 0x0f, 0, 0},

{0x5818, 0x0a, 0, 0}, {0x5819, 0x05, 0, 0}, {0x581a, 0x01, 0, 0},

{0x581b, 0x00, 0, 0}, {0x581c, 0x00, 0, 0}, {0x581d, 0x03, 0, 0},

{0x581e, 0x08, 0, 0}, {0x581f, 0x0c, 0, 0}, {0x5820, 0x0a, 0, 0},

{0x5821, 0x05, 0, 0}, {0x5822, 0x01, 0, 0}, {0x5823, 0x00, 0, 0},

{0x5824, 0x00, 0, 0}, {0x5825, 0x03, 0, 0}, {0x5826, 0x08, 0, 0},

{0x5827, 0x0c, 0, 0}, {0x5828, 0x0e, 0, 0}, {0x5829, 0x08, 0, 0},

{0x582a, 0x06, 0, 0}, {0x582b, 0x04, 0, 0}, {0x582c, 0x05, 0, 0},

{0x582d, 0x07, 0, 0}, {0x582e, 0x0b, 0, 0}, {0x582f, 0x12, 0, 0},

{0x5830, 0x18, 0, 0}, {0x5831, 0x10, 0, 0}, {0x5832, 0x0c, 0, 0},

{0x5833, 0x0a, 0, 0}, {0x5834, 0x0b, 0, 0}, {0x5835, 0x0e, 0, 0},

{0x5836, 0x15, 0, 0}, {0x5837, 0x19, 0, 0}, {0x5838, 0x32, 0, 0},

{0x5839, 0x1f, 0, 0}, {0x583a, 0x18, 0, 0}, {0x583b, 0x16, 0, 0},

{0x583c, 0x17, 0, 0}, {0x583d, 0x1e, 0, 0}, {0x583e, 0x26, 0, 0},

{0x583f, 0x53, 0, 0}, {0x5840, 0x10, 0, 0}, {0x5841, 0x0f, 0, 0},

{0x5842, 0x0d, 0, 0}, {0x5843, 0x0c, 0, 0}, {0x5844, 0x0e, 0, 0},

{0x5845, 0x09, 0, 0}, {0x5846, 0x11, 0, 0}, {0x5847, 0x10, 0, 0},

{0x5848, 0x10, 0, 0}, {0x5849, 0x10, 0, 0}, {0x584a, 0x10, 0, 0},

{0x584b, 0x0e, 0, 0}, {0x584c, 0x10, 0, 0}, {0x584d, 0x10, 0, 0},

{0x584e, 0x11, 0, 0}, {0x584f, 0x10, 0, 0}, {0x5850, 0x0f, 0, 0},

{0x5851, 0x0c, 0, 0}, {0x5852, 0x0f, 0, 0}, {0x5853, 0x10, 0, 0},

{0x5854, 0x10, 0, 0}, {0x5855, 0x0f, 0, 0}, {0x5856, 0x0e, 0, 0},

{0x5857, 0x0b, 0, 0}, {0x5858, 0x10, 0, 0}, {0x5859, 0x0d, 0, 0},

{0x585a, 0x0d, 0, 0}, {0x585b, 0x0c, 0, 0}, {0x585c, 0x0c, 0, 0},

{0x585d, 0x0c, 0, 0}, {0x585e, 0x0b, 0, 0}, {0x585f, 0x0c, 0, 0},

{0x5860, 0x0c, 0, 0}, {0x5861, 0x0c, 0, 0}, {0x5862, 0x0d, 0, 0},

{0x5863, 0x08, 0, 0}, {0x5864, 0x11, 0, 0}, {0x5865, 0x18, 0, 0},

{0x5866, 0x18, 0, 0}, {0x5867, 0x19, 0, 0}, {0x5868, 0x17, 0, 0},

{0x5869, 0x19, 0, 0}, {0x586a, 0x16, 0, 0}, {0x586b, 0x13, 0, 0},

{0x586c, 0x13, 0, 0}, {0x586d, 0x12, 0, 0}, {0x586e, 0x13, 0, 0},

{0x586f, 0x16, 0, 0}, {0x5870, 0x14, 0, 0}, {0x5871, 0x12, 0, 0},

{0x5872, 0x10, 0, 0}, {0x5873, 0x11, 0, 0}, {0x5874, 0x11, 0, 0},

{0x5875, 0x16, 0, 0}, {0x5876, 0x14, 0, 0}, {0x5877, 0x11, 0, 0},

{0x5878, 0x10, 0, 0}, {0x5879, 0x0f, 0, 0}, {0x587a, 0x10, 0, 0},

{0x587b, 0x14, 0, 0}, {0x587c, 0x13, 0, 0}, {0x587d, 0x12, 0, 0},

{0x587e, 0x11, 0, 0}, {0x587f, 0x11, 0, 0}, {0x5880, 0x12, 0, 0},

{0x5881, 0x15, 0, 0}, {0x5882, 0x14, 0, 0}, {0x5883, 0x15, 0, 0},

{0x5884, 0x15, 0, 0}, {0x5885, 0x15, 0, 0}, {0x5886, 0x13, 0, 0},

{0x5887, 0x17, 0, 0}, {0x3710, 0x10, 0, 0}, {0x3632, 0x51, 0, 0},

{0x3702, 0x10, 0, 0}, {0x3703, 0xb2, 0, 0}, {0x3704, 0x18, 0, 0},

{0x370b, 0x40, 0, 0}, {0x370d, 0x03, 0, 0}, {0x3631, 0x01, 0, 0},

{0x3632, 0x52, 0, 0}, {0x3606, 0x24, 0, 0}, {0x3620, 0x96, 0, 0},

{0x5785, 0x07, 0, 0}, {0x3a13, 0x30, 0, 0}, {0x3600, 0x52, 0, 0},

{0x3604, 0x48, 0, 0}, {0x3606, 0x1b, 0, 0}, {0x370d, 0x0b, 0, 0},

{0x370f, 0xc0, 0, 0}, {0x3709, 0x01, 0, 0}, {0x3823, 0x00, 0, 0},

{0x5007, 0x00, 0, 0}, {0x5009, 0x00, 0, 0}, {0x5011, 0x00, 0, 0},

{0x5013, 0x00, 0, 0}, {0x519e, 0x00, 0, 0}, {0x5086, 0x00, 0, 0},

{0x5087, 0x00, 0, 0}, {0x5088, 0x00, 0, 0}, {0x5089, 0x00, 0, 0},

{0x302b, 0x00, 0, 0}, {0x3503, 0x07, 0, 0}, {0x3011, 0x08, 0, 0},

{0x350c, 0x02, 0, 0}, {0x350d, 0xe4, 0, 0}, {0x3621, 0xc9, 0, 0},

{0x370a, 0x81, 0, 0}, {0x3803, 0x08, 0, 0}, {0x3804, 0x05, 0, 0},

{0x3805, 0x00, 0, 0}, {0x3806, 0x02, 0, 0}, {0x3807, 0xd0, 0, 0},

{0x3808, 0x05, 0, 0}, {0x3809, 0x00, 0, 0}, {0x380a, 0x02, 0, 0},

{0x380b, 0xd0, 0, 0}, {0x380c, 0x08, 0, 0}, {0x380d, 0x72, 0, 0},

{0x380e, 0x02, 0, 0}, {0x380f, 0xe4, 0, 0}, {0x3810, 0xc0, 0, 0},

{0x3818, 0xc9, 0, 0}, {0x381c, 0x10, 0, 0}, {0x381d, 0xa0, 0, 0},

{0x381e, 0x05, 0, 0}, {0x381f, 0xb0, 0, 0}, {0x3820, 0x00, 0, 0},

{0x3821, 0x00, 0, 0}, {0x3824, 0x11, 0, 0}, {0x3a08, 0x1b, 0, 0},

{0x3a09, 0xc0, 0, 0}, {0x3a0a, 0x17, 0, 0}, {0x3a0b, 0x20, 0, 0},

{0x3a0d, 0x02, 0, 0}, {0x3a0e, 0x01, 0, 0}, {0x401c, 0x04, 0, 0},

{0x5682, 0x05, 0, 0}, {0x5683, 0x00, 0, 0}, {0x5686, 0x02, 0, 0},

{0x5687, 0xcc, 0, 0}, {0x5001, 0x7f, 0, 0}, {0x589b, 0x06, 0, 0},

{0x589a, 0xc5, 0, 0}, {0x3503, 0x00, 0, 0}, {0x3010, 0x10, 0, 0},

{0x460c, 0x20, 0, 0}, {0x460b, 0x37, 0, 0}, {0x471c, 0xd0, 0, 0},

{0x471d, 0x05, 0, 0}, {0x3815, 0x01, 0, 0}, {0x3818, 0x00, 0x08, 0},

{0x501f, 0x00, 0, 0}, {0x4300, 0x30, 0, 0}, {0x3002, 0x1c, 0, 0},

{0x3819, 0x80, 0, 0}, {0x5002, 0xe0, 0, 0},

};

Weidong

0 Kudos
Reply
4,593 Views
johnturnur
Contributor III

thanks but it does not work for me. is there anything more needs to change other than this table?

Is there anything needs to change in IPU code to avoid flickers?

J

0 Kudos
Reply
4,593 Views
weidong_sun
NXP TechSupport
NXP TechSupport

Hello,John,

     Did you get OV5642 datasheet form OV company ? if not, please ask their support for document !

Weidong

0 Kudos
Reply