OV5640 camera not detected

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

OV5640 camera not detected

11,551件の閲覧回数
aravinthkumarja
Senior Contributor II

Hi All,

I'm using OV5640 mipi camera in imx6 and I'm getting below error.

[ 2.004525] ov564x_mipi 3-003c: found pwm2, period=0
[ 2.296520] ov5640_read_reg:write reg error:reg=300a
[ 2.296522] camera ov5640_mipi is not found

What is the reason for this error.?

How to fix this.

Regards,

Aravinth 

ラベル(4)
0 件の賞賛
返信
7 返答(返信)

10,568件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Aravinth 

issue may be related to i2c problems, one can try to debug it using

Chapter 19 OmniVision Camera Driver attached Linux manual.

i2c also can be tested using baremetal sdk found on SMP Enable in IMX6 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

10,568件の閲覧回数
aravinthkumarja
Senior Contributor II

Hi igor,

Thanks for your response. I have configured as mentioned in document. But I don't know why I'm facing this issue.?

Regards,

Aravinth

0 件の賞賛
返信

10,568件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Aravinth

>But I don't know why I'm facing this issue

reason may be that i2c is not working

Best regards
igor

0 件の賞賛
返信

10,568件の閲覧回数
aravinthkumarja
Senior Contributor II

Hi igor,

I2C interface and camera both are working, I have validated in linux BSP and camera driver as module (.ko).

If I make it as inbuilt it's not working in linunx BSP. In Android BSP camera not at all working in both module and inbuilt build. 

Regards.

Aravinth

0 件の賞賛
返信

10,568件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Aravinth

if i2c is working one can try to debug it in camera driver described in sect.6.1.8

Source Code Structure attached Linux Manual.

Best regards
igor

0 件の賞賛
返信

10,568件の閲覧回数
aravinthkumarja
Senior Contributor II

Thanks igor, It's default driver code. 

Finally I have fixed that issue. 

Regards,

Aravinth

0 件の賞賛
返信

10,568件の閲覧回数
leeshuai
Contributor III

Hi Aravinth

          How do you fixed that issue?

0 件の賞賛
返信