OTA Bootloader Updates

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

OTA Bootloader Updates

1,693 Views
michaelrobbelot
Contributor IV

Anyone,

I was wondering if it was possible to use OTA to update the bootloader and if so, what the recommended changes are to enable this to occur. I know section 5.7 of the Android Advanced guide (ICS BSP) discusses how to modify the update archive to update the bootloader via recovery, but was wondering about its applicability to OTA. Also, the instructions for modifying the update zip are a little vague when it mentions, "...you need to perform some sys file operation before dd," -- it would be great to know what this means exactly. I would prefer to make the changes to the ota_from_target_files script rather than do something after the fact as is mentioned with update archive (why isn't the recommended path to update source files bootable/recovery?). Thanks.

Michael Robbeloth

Labels (2)
0 Kudos
Reply
1 Reply

1,422 Views
jamesbone
NXP TechSupport
NXP TechSupport

For the i.MX53 ICS Android BSP  I do not think we have this option available,  as you can see in the following thread even do, it is from a previous one. Since only for i.MX6 JellyBean 4.2.2.1 it is in the package release.

How to enable the OTA update feature in Android r10.3 release?

0 Kudos
Reply