ONOFFpin debounce time

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

ONOFFpin debounce time

ソリューションへジャンプ
2,144件の閲覧回数
goto11
Contributor III

hello,Community

The i.MX 7 Dual Applications Processor Reference Manual Dumb PMIC mode is described as follows.

Debounce—the debounce configuration supports 0 ms, 50 ms, 100 ms, and 500 ms.
The debounce is used to generate the set_pwr_off_irq interrupt. While it is in the ON state and the button is pressed longer than the debounce time, the set_pwr_off_irq is generated.

On the other hand, Figure 6-7. About FSM
The condition for transition from the OFF state is described as button pressed (any duration).
Can the debounce time be set in the same register for the transition from the ON state and the transition from the OFF state?

best regards

Goto

ラベル(1)
0 件の賞賛
返信
1 解決策
2,027件の閲覧回数
gusarambula
NXP TechSupport
NXP TechSupport

Hello Goto,

The debounce mechanism works for both transitions as you can see in Figure 6-6. Once after the Power-On Reset the debounced is used to avoid false readings to turn ON and OFF, and it’s the one configured for the “power off” interrupt. It cannot be set independently for each transition.

I hope this helps!
Regards,

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,028件の閲覧回数
gusarambula
NXP TechSupport
NXP TechSupport

Hello Goto,

The debounce mechanism works for both transitions as you can see in Figure 6-6. Once after the Power-On Reset the debounced is used to avoid false readings to turn ON and OFF, and it’s the one configured for the “power off” interrupt. It cannot be set independently for each transition.

I hope this helps!
Regards,

0 件の賞賛
返信