ONOFFpin debounce time

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ONOFFpin debounce time

Jump to solution
2,143 Views
goto11
Contributor III

hello,Community

The i.MX 7 Dual Applications Processor Reference Manual Dumb PMIC mode is described as follows.

Debounce—the debounce configuration supports 0 ms, 50 ms, 100 ms, and 500 ms.
The debounce is used to generate the set_pwr_off_irq interrupt. While it is in the ON state and the button is pressed longer than the debounce time, the set_pwr_off_irq is generated.

On the other hand, Figure 6-7. About FSM
The condition for transition from the OFF state is described as button pressed (any duration).
Can the debounce time be set in the same register for the transition from the ON state and the transition from the OFF state?

best regards

Goto

Labels (1)
0 Kudos
Reply
1 Solution
2,026 Views
gusarambula
NXP TechSupport
NXP TechSupport

Hello Goto,

The debounce mechanism works for both transitions as you can see in Figure 6-6. Once after the Power-On Reset the debounced is used to avoid false readings to turn ON and OFF, and it’s the one configured for the “power off” interrupt. It cannot be set independently for each transition.

I hope this helps!
Regards,

View solution in original post

0 Kudos
Reply
1 Reply
2,027 Views
gusarambula
NXP TechSupport
NXP TechSupport

Hello Goto,

The debounce mechanism works for both transitions as you can see in Figure 6-6. Once after the Power-On Reset the debounced is used to avoid false readings to turn ON and OFF, and it’s the one configured for the “power off” interrupt. It cannot be set independently for each transition.

I hope this helps!
Regards,

0 Kudos
Reply