ONOFF Pin Input Voltage Level

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ONOFF Pin Input Voltage Level

1,474 Views
sadatanvashisth
Contributor II

Can any one let me know what is the minimum VIH and maximum VIL for ONOFF pin of IMX6UL?

Labels (1)
Tags (1)
0 Kudos
Reply
1 Reply

1,317 Views
gusarambula
NXP TechSupport
NXP TechSupport

Hello Sadatan Vashistha,

The ONOFF Pin is on the VDD_SNVS_IN power domain and is a GPIO ball type, so according to the datasheet on table 24 (Single Voltage GPIO DC Parameters), it would be:

ParameterSymbolTest ConditionsMinMaxUnits
High-Level input voltageVIH —0.7 × OVDDOVDDV
Low-Level input voltage VIL—00.3 × OVDDV

Where OVDD would be VDD_SNVS_IN.


I hope this helps!
Regards,

0 Kudos
Reply