ONOFF Pin Input Voltage Level

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

ONOFF Pin Input Voltage Level

1,525件の閲覧回数
sadatanvashisth
Contributor I

Can any one let me know what is the minimum VIH and maximum VIL for ONOFF pin of IMX6UL?

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 返信

1,368件の閲覧回数
gusarambula
NXP TechSupport
NXP TechSupport

Hello Sadatan Vashistha,

The ONOFF Pin is on the VDD_SNVS_IN power domain and is a GPIO ball type, so according to the datasheet on table 24 (Single Voltage GPIO DC Parameters), it would be:

ParameterSymbolTest ConditionsMinMaxUnits
High-Level input voltageVIH —0.7 × OVDDOVDDV
Low-Level input voltage VIL—00.3 × OVDDV

Where OVDD would be VDD_SNVS_IN.


I hope this helps!
Regards,

0 件の賞賛
返信