I want to test PCIe eye pattern for i.MX7 Dual core.
Can you tell me the method of PCIe eye pattern test?
Thank you.
Best Regards,
Alex Cheng
Hi Alex
one can try to follow sect.2.1 TX test configuration and procedures
AN4784 PCIe Certification Guide
https://www.nxp.com/docs/en/application-note/AN4784.pdf
according to footnote 2 on p.3 :
2. After a far-end termination is determined to be present, the Link Training and
Status State Machine (LTSSM) enters the polling.compliance state and begins transmitting
the compliance pattern on all lanes. Users do not need to enter
any command to force the system into the polling.compliance state after boot.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------