ODT setting

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

ODT setting

2,528件の閲覧回数
sparkyee
Contributor I

Hi,

     I have  successfully finished SI and timing closure using Hyperlynx 9.3 simulation tool. The tool requires

me to enable (ddr3_odt_t60_sel11_mi) ODT settings for read accesses from the memory to the MMDC controller. I want to know if this is accomplished in the MPODTCTRL register (0x021B01818) or in a IOMUX_SW_PAD_CTL_PAD_DRAM_xxxx register? Also in the Programming AID Ver 1.9 the MPODTCTRL register seems to have ODT disabled for READ accesses since the lower 4 bits are set to "7"? I have read all of the ODT threads here and there seems to be a lot confusion about setting ODT properly. I have used Hyperlynx on iMX31 and

iMX53 designs before and have had excellent correlation to the physical design. I want to make sure I translate the simulation output into correct register settings in the initialization code. My design emulates the Sabre SD board but

was laid out in Expedition instead or Cadence allegro. Thanks for your help!

ラベル(1)
0 件の賞賛
返信
1 返信

2,380件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Larry

ODT settings of IOMUX are for the DDR Address and control pins,

and the ODT settings of MMDCx_MPODTCTRL are for the Data bus (by byte group).

So you can controls the ODT value for each byte group by the ODTx_INT_RES.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信