Noise Reduction algorithm running on IMX6 for Audio Codec

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Noise Reduction algorithm running on IMX6 for Audio Codec

1,887件の閲覧回数
mujeebshaik
Contributor II

Hi,

Can anyone help me out to fix the follwing issue,

We are using Audio CODEC from Wolfson micro WM8960  with Single ended MIC and One channel Speaker ( 8 Ohm – 1 to 1.5W rating),We are getting huge noise on the speaker when MIC is activated simultaneously,System works Ok if either of them i.e. MIC or Speaker is active.

0 件の賞賛
返信
1 返信

1,599件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

http://www.wolfsonmicro.com/documents/uploads/misc/en/WAN0129.pdf

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信