Noise Reduction algorithm running on IMX6 for Audio Codec

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Noise Reduction algorithm running on IMX6 for Audio Codec

1,865 Views
mujeebshaik
Contributor II

Hi,

Can anyone help me out to fix the follwing issue,

We are using Audio CODEC from Wolfson micro WM8960  with Single ended MIC and One channel Speaker ( 8 Ohm – 1 to 1.5W rating),We are getting huge noise on the speaker when MIC is activated simultaneously,System works Ok if either of them i.e. MIC or Speaker is active.

0 Kudos
Reply
1 Reply

1,577 Views
igorpadykov
NXP Employee
NXP Employee

http://www.wolfsonmicro.com/documents/uploads/misc/en/WAN0129.pdf

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply