Nodejs do_compile fails.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Nodejs do_compile fails.

818 次查看
MginoM
Contributor I

Hi all,

I'm a bit new to creating images so I'm running into multiple errors which I have been resolving.  Now, I have run into an error that I can't resolve.

Host Machine is running Ubuntu 20.04

Target machine is imx8 mini.

distro is fsl_imx_xwayland

machine is imx8mevk

image is imx_image_multimedia.

I was able to create the image successfully without nodejs.

When I try to create same image but adding IMAGE_INSTALL:append = " nodejs" to local.conf the compilation fails with exit code "1".  Same error if I attempt to compile nodejs recipe by itself.

the bb file indicates that the nodejs version is 16.11.1.

Any ideas on how to resolve this issue?

thanks,

 

 

标签 (1)
0 项奖励
回复
0 回复数